STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

going back to legacy, but can't

Posted on September 23, 2015 at 18:03Please help me. I am trying t go back to using the legacy standard peripheral library (no Cube) like I used to.When I try to build a project, I follow the readme file and include the stm324xg_eval files in the pr...

estersci2 by Associate III
  • 1777 Views
  • 5 replies
  • 0 kudos

stm32f103xx+w5100

Posted on September 23, 2015 at 12:59i want to run the w5100 with stm32103xx. I wonder if It is possible. Is there  any solution for this? thanks a lot #spi #stm32f103 #w5100

mehran by Associate
  • 1642 Views
  • 1 replies
  • 0 kudos

SWD not working on STM32F303RET6

Posted on September 22, 2015 at 23:51Hi all, My problem is quite unusual, and I need some new ideas. I can't make SWD connection working on STM32F303RET6. I'm constantly getting ''Can not connect to target'' message. I have installed the latest ve...

STM32L151 and microSD card

Posted on September 24, 2015 at 01:10Hi,I want to connect a microSD card to my STM32L151CBU6 MCU and read/write data to this uSD card. I have made the schematics, but I am unsure if I have connected the uSD card holder correctly to the MCU (see atta...

0690X000006031MQAQ.jpg
lrsolem by Associate
  • 1111 Views
  • 0 replies
  • 0 kudos

Forum acting quirky today

Posted on September 17, 2015 at 19:00Not sure if ST changed some settings, but I'm getting a lot of errors when posting, or when I open an new tab against a link (ie navigating back to a post from hyperlinks provided on the page, or edit window, to ...

cubexmx usb hid code generation for stm32f411

Posted on September 02, 2015 at 23:10 Hi I have a custom board with a stm32f4 I am trying to use cubmx to generate a usb HID project but the generated code does not work. The board appears as an unrecognized device when I attach it to my com...

0690X00000604WWQAY.png 0690X00000604s6QAA.png
ruairi by Associate
  • 2852 Views
  • 5 replies
  • 0 kudos

STM32F4xx RTC questions

Posted on September 21, 2015 at 16:49All:First, I have been able to ''setdatetime'' and ''getdatetime'' using excellent example code. In fact, I wait until after powered up to receive a ''setdatetime'' command (via UART). Using the HSE on F4 Discove...

tba10596 by Associate II
  • 2121 Views
  • 3 replies
  • 0 kudos

STM32L476QE Flash write and Erase API

Posted on September 10, 2015 at 14:12We are using STM32LL476QE and as per reference manual , While executing a program code from bank 1, it is possible to perform a program operation on the bank 2. Here we are into situation in which Our custom Boot...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.