STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Can-Bus Problem

Posted on October 09, 2015 at 22:37The original post was too long to process during our migration. Please click on the attachment to read the original post.

PLC on STM32 idea

Posted on May 22, 2012 at 11:49Some companies have PLC softwares (like as IEC 61131-3 Development System CoDeSys) that have a runtime core that can be programmed on STM32 micros and we can write PLC programs and download it to stm32 without any C co...

STM32F411Ediscovery Firmware

Posted on April 22, 2015 at 18:51There is really very little available for the STM32F411Ediscovery board. WHere can I find the default software (hex file) to put the board back to default? #stm32f411

vector table location

Posted on July 12, 2012 at 07:09hi, i search and search but i cant find where i can change Vector Table base location in memory.map i can find .text 0x08004000 0x718  *(.isr_vector .isr_vector.*)  .isr_vector 0x08004000 0x124 ..\obj\startup_stm32f...

redkofka by Associate II
  • 9925 Views
  • 12 replies
  • 0 kudos

ethernet communication

Posted on October 10, 2015 at 09:37Dear Sir/MadamI am using modbus TCP/IP protocol using ethernet card , the issue is when ever i unplug the ethernet cable manually with out power off and reinsert the same the communication between the modbus and et...

i2c combined example

Posted on October 10, 2015 at 16:53Hi,I would be very grateful if anyone could post some sample code to implement... i2c 7-bit protocol with combined  write and read, multiple data bytes to be read in a sequence.Basic std FW library compatible sampl...

estersci2 by Associate III
  • 1453 Views
  • 2 replies
  • 0 kudos

Instructions SVC (ARM)

Posted on September 29, 2015 at 22:18__asm ??volatile (''SVC 0x4''); code08000D7A svc 4; debugger AssemblerAnd even in the final bin contains 4 SVC team in the junior ranks.0x4 - (0x0 ~ 0x255) - should be added to the current ''PC'' register at the ...

Unsigned char is always true ?

Posted on October 10, 2015 at 03:06Guys, What should I change for fixing : Warning : comparison of constant 49152 with expression of type ''unsigned char'' is always true ....? the line is : while(Mp3ReadRegister(0x03) != CLOCK_REG) .... unsigned ch...

Timer-Synch + IRQ-Jitter

Posted on October 09, 2015 at 11:33Hello I've a question regarding the timer synchronization on an STM32L4. I've setup TIM1 and TIM8 to run in synch triggered by TIM2. To test the code I simply toggle a pin inside the TIM1 and TIM8 update interrupts...

0690X000006059tQAA.png 0690X00000605DKQAY.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.