STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 - Hanging on SPI Get Status

Posted on October 11, 2015 at 23:36Hi, I'm trying to get a Micron M25P128 flash device going on SPI1. below is the initialization, and then the send function. At this point I am sending just a read ID opcode, but it is hanging at the next line after...

[Bug] SAI1 PLL settings CubeMX

Posted on September 11, 2015 at 16:13 Hello There is a bug in the current version of CubeMX using the L4 libs. The ''PLLSAI1ClockOut'' (and I assume the SAI2 one) isn't set within the generated SystemClock_Config function which leads to ...

STM32F4 Delay

Posted on October 31, 2014 at 16:29Hello.How to insert precision delay with timer or systick?For example, 100 ns or 1 us.Best regards,CH

CubeMX tool generates dubious declaration for periph init.

Posted on September 27, 2015 at 16:07Hi, when I generate code for the STM32L0 in CubeMX, my compiler discovers the following problem:~/projecten/SunnaBat/software/Controller/toepassing/cube/SunnaBat/Src/adc.c:149:47: error: declaration of 'hadc' sha...

Any example program for STM32F411E-DISCO discovery?

Posted on April 16, 2015 at 10:33Hi, I bought a STM32F411EDISCOVERY instead of STM32F4Discovery board. I found the STM32F4-Discovery demo program the STMCube firmware package is for STM32F407 target only. What should I do to make it compatible to ST...

How to compare a result of a function ?

Posted on October 11, 2015 at 12:39Guys, How can compare the result of the furnction output ? I have on main.c :Code:result = VS1053_Init(); if (result == 0) { HAL_GPIO_WritePin(GPIOE, GPIO_PIN_6 , 1 ); HAL_Delay(100); HAL_GPIO_WritePin(GPIOE, GPIO...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.