STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where is TIM_GetITStatus() documented?

Posted on October 14, 2015 at 22:57I'm using the STM32F0308-DISCO board and want to have an interrupt generated on both edges of a PWM (generated by TIM15).  Using STM32CubeMX, I found how to generate the TIM15_IRQHandler.  Then, a search here showe...

STM32F030 Internal Timers

Posted on October 14, 2015 at 22:01I have an application where an external rising edge triggers timer 15 on PA2(pin 16) used in its input capture and compare mode. Then slave timer 3 from timer 15 to clock the internal ADC receiving data on PA0 (pin...

Problem with FATFS File System on nucleo Board L152RE

Posted on October 14, 2015 at 16:03Hi,I would like to know if it's possible to use FATFS file system on a nucleo L152RE without using memory card.I just want to use the flash of the nucleo board but i need to save some informations with three fields...

STM32F401RET6 - Nucleo Board - SPI Problems

Posted on October 14, 2015 at 00:53 I have been working on setting up and trying to test the SPI output from the Nucleo-F401RE. I am currently using a logic analyzer to view the data and clock lines, though I have not yet been able to see any ch...

kyleprice by Associate II
  • 1187 Views
  • 2 replies
  • 0 kudos

Watchdog reset while changing CLock frequency

Posted on October 14, 2015 at 16:13I have configured my stm32f427 microcontroller,  Sysclk to run in a clock frequency of 60mhz(HSI and PLL). I have reduced it to 16mhz (Sysclk directly from HSI). While executing this code watchdog resets. Below men...

jijo137 by Associate II
  • 1373 Views
  • 2 replies
  • 0 kudos

SPI readout of a sensor

Posted on October 12, 2015 at 01:55Hi, I am trying a very simple thing: I would like to read a register of a sensor. So the first thing I did is to write the read-register (8 bit) to the sensor. After that the DR register has been filled with dummy...

USART RX interrupt driven ring buffer

Posted on October 14, 2015 at 08:51Hey guys. First of all im new to this kind of stuff, so dont judge me please. I've been working for days on USART. I learned to transmit and receive strings via usart in normal mode, but as i try to do it with inte...

e239955 by Associate II
  • 3659 Views
  • 5 replies
  • 0 kudos

Multiple ADC STM32F303 discovery board

Posted on July 09, 2013 at 23:45The original post was too long to process during our migration. Please click on the attachment to read the original post.

marko by Associate II
  • 4995 Views
  • 10 replies
  • 0 kudos

I2C on stm32f301

Posted on October 06, 2015 at 11:50I've started development of an application on an STM32F3 discovery baord, and am moving onto the target board, which uses an STM32F301. I can't get the I2C peripherals to run. If can bit-bash I2C on the GPIO, but ...

artgodwin by Associate II
  • 1198 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.