2015-10-06 2:50 AM
I've started development of an application on an STM32F3 discovery baord, and am moving onto the target board, which uses an STM32F301.
I can't get the I2C peripherals to run. If can bit-bash I2C on the GPIO, but not use the integrated parts. These (at least, some of them) were OK on the 303 on the discovery board. I've gone through the configuration registers and changed everything as far as I can see them but I'm apparently missing something. The pins don't clock, and the transfers time out. Any idea what I should look at ? Is there some critical difference between 301 and 303 that I'm missing ? It's very difficult to find online information about the 301 and some of the example code doesn't support it. Is it a dead end ?2015-10-08 7:43 AM
Hi artag,
You have to refer to STM32F301http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00093332.pdf
in order to know exact pins to be used for your I2C.F3 Discovery boards embed an LQFP100 package, while we have LQFP64 packages for STM32F301. For sure some pins are no more available.Which package and which I2C instance are you using exactly?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-10-14 7:17 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.