STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Merge SDIO with FATFS

Posted on October 21, 2015 at 13:33Hi,I have created a sdio and i would like to know how to merge the FATFS file system with the SDIO. I have seen some examples but  i am not understanding how the they give a link between file system module and SDIO...

arunease by Associate II
  • 3154 Views
  • 10 replies
  • 0 kudos

SDRAM STM32F429 FMC SDRAM DELAY

Posted on May 10, 2015 at 22:47The original post was too long to process during our migration. Please click on the attachment to read the original post.

Use USB CDC with DMA?

Posted on October 23, 2015 at 17:49Is there a way to use the USB stack of the F4Disco with DMA? I'd like to transfer some 100 bytes and then trigger an interrupt... At the moment I'm using UART with a USB-UART bridge for that.

Leonelf by Associate II
  • 3312 Views
  • 1 replies
  • 1 kudos

Can't get Multiple ADCs working on STM32F303VCT6

Posted on April 01, 2015 at 22:11Hi, I am using the STM32F303VCT6 chip on the STM32F3Discovery Kit. I want to use 37 of the 39 available ADC inputs for a data logger project. I have successfully got ADC1 working with DMA1_Channel1 and ADC2 working ...

STemWin VNC + Anti Alias

Posted on October 26, 2015 at 08:33Hi,using STemWin, I encountered the following problem. Anti aliasing is working fine until the VNC server process is started. Then, some of the AA routines don't work anymore, e.g. GUI_AA_DrawLine doesn't do anythi...

gsiebke by Associate II
  • 665 Views
  • 0 replies
  • 0 kudos

Is DMA Circular mode working in STM32F746G-Disco?

Posted on September 13, 2015 at 21:29 Hi, I have a project in STM32F746G-Disco with its SPDIFRX interface. I was able to use STM32CubeMX to generate the intializations and the sceleton project. As it is right now, I can receive ...

sv1eia by Associate II
  • 2045 Views
  • 6 replies
  • 0 kudos

BLDC Motor is locked when using STM32 PMSM FOC LIBv4.2

Posted on October 26, 2015 at 07:07Hi everybodyI am using STM32 PMSM FOC LIBv4.2 to turn a three phase 60V/350W BLDC motor with Pole pair=28 and rated speed=265rpm. I am using Hall sensor to detect rotor position/speed and Single Shunt current measu...

Custom USART for STM32103VE

Posted on October 16, 2015 at 05:23Hello.I have to use asynchronous and synchronous modes. For asynchronous, I'm already using the built-in USART peripheral. My problem is the synchronous one. My clock needs to be 16 ticks per bit and more important...

Using two UART

Posted on October 21, 2015 at 20:31Hello,I using STM periph. library and I would need to use two UARTs on STM32F103. One UART for serial Modbus RTU comunication with sensors and one UART for terminal interface which will show data from sensors and p...

hospodar by Associate III
  • 2392 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.