2015-10-15 8:23 PM
Hello.
I have to use asynchronous and synchronous modes. For asynchronous, I'm already using the built-in USART peripheral. My problem is the synchronous one. My clock needs to be 16 ticks per bit and more importantly, I should use the same pins for RX and TX for the two modes.The only solution that I can think of is to just use the GPIO pins and create the waveform myself. May I know if there is an easier way compared to this?Thanks. #usart #stm322015-10-15 8:56 PM
One clock for both, or independent clocks for Tx and Rx? Who generates the clock(s)?
EXTI interrupts sending/receiving bits? DMA+TIM+GPIO outputting pin sequences from a pattern buffer?2015-10-15 10:25 PM
Hello. Same CLK for RX and TX and generated by stm32.
I don't know yet EXTI Interrupts and DMA. I'll read about them.2015-10-25 12:27 AM
Hello clive1, I tried GPIO only and Systick timer+GPIO but I can't reach 5 Mhz clock that is around 50% duty cycle. Is this even possible? Thanks.
2015-10-25 10:21 AM
Well how fast exactly do you expect/need this thing to be?
Perhaps if you're working with odd protocols, and data rates >1Mbps, you might consider doing it with a CPLD or FPGA? The F1 is a rather old part, where the GPIO is attached to a peripheral bus (APB), rather than a hardware bus (AHB). I suspect it might support signal pattern generation in the 8-9 MHz range. And interrupts up a few 100 KHz.2015-10-25 5:46 PM
5 Mhz is the clock I need. When toggling the clock pin alone, it is almost 40-50% duty cycle. But when I also modify the data pin, the clock seems random at 2-5 Mhz.
Unfortunately for me, CPLDA or FPGA is not possible.2015-10-25 6:06 PM
Should I try and imagine what you are doing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.