STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hou to use old package version on STM32CUBEMX

Posted on June 11, 2015 at 16:57Hi,I have the most current STM32CUBEMX version, 4.8.0. In this version I cannot choose the firmware package version that I want to use, it only allows to use the most current, but I want to use an  old version. Versio...

STM32F0- triggering DMA by a timer.

Posted on October 24, 2015 at 15:37  I want to have a timer trigger a DMA transfer. I have a STM32F072RB processor. I currently have TIM1 as the timer. I have the timer running and reloading and that seems to work. It is currently also triggering an...

Can't read the documents in nucleo_64pins_sch.zip

Posted on October 26, 2015 at 19:42I have a NUCLEO-F401RE board. I tried to find its connector pin out, because the schematic diagram is made with some hobby tool and useless. All the doc document files use some odd format I can't read opened. I tri...

LMI2 by Lead
  • 1293 Views
  • 2 replies
  • 0 kudos

CubeMX 4.9 and USB host + fatfs

Posted on August 21, 2015 at 21:31Hello! I apologize for my bad English, but I do not have anyone to ask. My task is to create a USB host to work with flash pametyu. I also use fatfs. I'm using a microcontroller STM32f407VG. To create a project I us...

[Solved] Discovery f429 USB Host (usb stick not working)

Posted on May 12, 2015 at 00:20Hi,I worked for several weeks on a dictaphone project with the board F429 discovery. The goal is to write the values ​​of the ADC to a file on a USB key.My ADC works with DMA, everything is ok.However, I generated my f...

raph by Associate
  • 1079 Views
  • 3 replies
  • 0 kudos

BSRR versus BSRRL and BSRRH

Posted on October 21, 2015 at 14:59Hello, why do the recent STM32Cube Headers  still keep BSRRH/BSRRL in the GPIO_Typedef in STM32Cube_FW_F3_V1.3.0 while STM32Cube_FW_F2_V1.2.0 drops BSRRL/BSRRH in favour of BSRR as used in the other headers This ma...

STM32F0 Curious ADC behaviour

Posted on October 11, 2015 at 15:07This is relation to my previous forum post [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F030F4%20ADC%20strange%20behavio...

srdjan by Associate II
  • 7915 Views
  • 10 replies
  • 0 kudos

__HAL_TIM_GET_FLAG

Posted on October 27, 2015 at 11:37hello everybody !!! I'm using ''__HAL_TIM_GET_FLAG'' on my STM32l051K6 for detect an overflow on my timer, but i don't know how much machine cycle it takes ?Could someone tell me how this function uses machine cycl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.