STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030R8T6 and STM32F091RC pin to pin compatibility

Posted on October 23, 2015 at 09:46Good morning, i've already working with a STM32F030R8T6 MCU but i need more flash memory.Is STM32F091RC pin to pin compatible with no code changes?There is a MCU similar to STM32F030R8T6 but with more than 64K Flas...

pietro2 by Associate II
  • 1499 Views
  • 2 replies
  • 0 kudos

ST presented STM32 Nucleo-32

Posted on October 15, 2015 at 11:16It seems ST renamed the old STM32 Nucleo borads to STM32 Nucleo-64, and presented new STM32 Nucleo-32 boards which are smaller than the original ones. http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1847

DAC and DMA with STM32L0 Nucleo

Posted on October 13, 2015 at 18:20Hello, Newbee, I'm trying to generate sinewave at 1Khz using DAC and DMA on my STM32L0R53 Nucleo Board. I'm using STM32CubeMx to initialise DAC and DMA but doesn't work. Where can I find tutorial or sample code? S...

STM32F030 first board

Posted on October 28, 2015 at 09:34Hi to all, I would like to create my own board using a STM32F030K6T6, but I have some doubts about sending the program from PC to MCU flash. According to datasheet I should tie BOOT0 to '1' and use PA2 and PA3 (USA...

STM32 bootloader issue

Posted on October 28, 2015 at 13:17Hi!At our company we are using STM32F205 in as a USB module. Connecting the USART3 to an FTDI converter. The MCU is then regulated to 3v and the FTDI is powered direcly from USB 3.3v. BOOT pins are set to stay in b...

mikael2 by Associate II
  • 1221 Views
  • 1 replies
  • 0 kudos

Where is the AN4024 application note ?

Posted on October 27, 2015 at 19:25Hi, I've just douwnloaded the software from this page : http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257935 Its release_notes file deals with AN4024 ''STM32 secure firmware upgrade (SFU...

JulienD by Senior
  • 1852 Views
  • 4 replies
  • 0 kudos

STM32F303RB Vrefint

Posted on October 01, 2015 at 08:16  The original post was too long to process during our migration. Please click on the attachment to read the original post.

Put one Buffer to SRAM1 and One Buffer to SRAM2

Posted on October 26, 2015 at 13:05HiThe aim of my project is recording stereo audio and send audio data by uart in real time.My device is STM32F405.I am using SPI2 as I2S Interface in Master Half Duplex in Receiving Mode.Sample rate = 8k and Data W...

razi by Associate
  • 2050 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.