STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 composite USB device

Posted on November 22, 2015 at 03:49I need to create UAC+CDC USB device. I have now two different projects with UAC and CDC implemented. How to organize them into composite device?My solution now is to describe device as  0x12,                      ...

Nucleo STM32F4012RE with StdPeriph USART Issue

Posted on November 21, 2015 at 13:26Hi,I've been trying to get USART working on my Nucleo board with the StdPeriph Libraries. (I haven't moved to HAL yet). Anyway, I have followed clive'1 post from [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32...

dman by Associate II
  • 1321 Views
  • 3 replies
  • 0 kudos

Vref - ADC accuracy

Posted on November 20, 2015 at 09:33Hi, Are there any software examples available about improving the ADC accuracy by using Vref? I’m trying to eliminate conversion errors due to Vref fluctuations. Thanks  

paul2 by Senior
  • 877 Views
  • 2 replies
  • 0 kudos

STM32Cube V1.9.0 F429 Demo bug

Posted on November 17, 2015 at 21:42HiIn the  STM32F429I-Discovery Demo STM32Cube\Repository\STM32Cube_FW_F4_V1.9.0\Projects\STM32F429I-Discovery\DemonstrationsThis demo worked the first couple of times, but then I've had this demo randomly fail whe...

st140728 by Associate II
  • 888 Views
  • 2 replies
  • 0 kudos

FSMC access speed

Posted on November 20, 2015 at 08:08HiI need to configure the FSMC in an STM32F4  to the fastest possible read access. I am reading an external FIFO and I need to read it as fast as it is possible. What are the parameters that influence the access s...

albertbu by Associate
  • 1321 Views
  • 2 replies
  • 0 kudos

STM32F4 FFT problem

Posted on November 19, 2015 at 15:36I have installed all DSP source files on the project and f32 fft works perfectly, but when I switch to q31 or q15, while  the input buffer shows got data, the output buffers all values (the frequency spectrum) are...

matas by Associate II
  • 2183 Views
  • 4 replies
  • 0 kudos

CubeMX version inconsistency

Posted on November 20, 2015 at 02:20As far as I know, the current version of CubeMX is 4.11.00. I'd downloaded the windows installer for the standalone version STM32CubeMX from http://www.st.com/web/en/catalog/tools/PF259242 and it works as expected...

STM32F4 fft to orginal signal amplitude confirmation

Posted on November 20, 2015 at 17:40Hey guys, I just need a confirmation, that I understood this correctly. To compute the orginal signals amplitude from the FFT amplitude, you have to divide the FFT specific frequency amplitude from the FFT length ...

matas by Associate II
  • 814 Views
  • 0 replies
  • 0 kudos

JLinkGDBServer Problem Write Accessing BKSPRAM and CCMRAM

Posted on November 20, 2015 at 17:37Hi All,I have recently moved over to using a Segger J-Link JTAG adapter. I'm using JLinkGDBServer, ARM Tools GDB in eclipse. The device on my target hardware is an STM32F427II. It appears that I only have R/W acce...

kirem by Associate II
  • 704 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.