cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo STM32F4012RE with StdPeriph USART Issue

dman
Associate II
Posted on November 21, 2015 at 13:26

Hi,

I've been trying to get USART working on my Nucleo board with the StdPeriph Libraries. (I haven't moved to HAL yet). Anyway, I have followed clive'1 post from [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/USART%20example%20code%20for%20Nucleo%20F401RE&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=1777]here  but it does not seem to work on my Nucleo and I cannot figure out why.

Here is what I've got:

/* Includes ------------------------------------------------------------------*/

#include ''stm32f4xx.h''

#include ''stm32f4xx_gpio.h''

#include ''stm32f4xx_i2c.h''

#include ''stm32f4xx_usart.h''

#include ''stdio.h''

#ifdef __GNUC__

  /* With GCC/RAISONANCE, small printf (option LD Linker->Libraries->Small printf

     set to 'Yes') calls __io_putchar() */

  #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)

#else

  #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)

#endif /* __GNUC__ */

/**

 * @brief  Wait till USART finishes transmission

 */

#define USART_WAIT(USARTx)                  do { while (!((USARTx)->SR & USART_FLAG_TXE)); } while (0)

static uint8_t buf[64];

/* Private function prototypes ----------------------------------*/

void Delay(__IO uint32_t nCount);

void GPIO_Configuration(void);

void Initialise_I2C(void);

void RCC_Configuration(void);

void RCC_Configuration(void)

{

  /* --------------------------- System Clocks Configuration -----------------*/

  

RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

}

 

/**************************************************************************************/

 

void GPIO_Configuration(void)

{

  GPIO_InitTypeDef GPIO_InitStructure;

  /* Connect USART pins to AF */

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);

 

  /*-------------------------- GPIO Configuration ----------------------------*/

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; // PA.2 USART2_TX, PA.3 USART2_RX

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_Init(GPIOA, &GPIO_InitStructure);

}

 

/**************************************************************************************/

 

void USART2_Configuration(void)

{

  USART_InitTypeDef USART_InitStructure;

 

  /* USARTx configuration ------------------------------------------------------*/

  /* USARTx configured as follow:

        - BaudRate = 9600 baud

        - Word Length = 8 Bits

        - One Stop Bit

        - No parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

  USART_InitStructure.USART_BaudRate = 9600;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

 

  USART_Init(USART2, &USART_InitStructure);

 

  USART_Cmd(USART2, ENABLE);

}

void OutString(char *str)

{

  /* Go through entire string */

while (*str) {

/* Wait to be ready, buffer empty */

USART_WAIT(USART2);

/* Send data */

USART2->DR = (uint16_t)(*str++ & 0x01FF);

/* Wait to be ready, buffer empty */

USART_WAIT(USART2);

}

}

/**

* @brief Main program

* @param None

* @retval None

*/

int main(void)

{

RCC_Configuration();

 

GPIO_Configuration();

 

USART2_Configuration();

OutString(''Hello World!'');

while (1)

{

Delay(0x000FF);

}

}

I can connect to COM port with no problem, but the output I am seeing is garbage: ''ððððððððððððððððððððððð''.

I've tried the example UART project that comes with STM32Cube and it works on the same USART2. 

I've also had my oscilloscope hooked to PA_2 and PA_3 but could not see anything. Not sure if its my scope not picking anything or some settings on it are wrong.

Any advice would be appreciated.

Thanks
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on November 21, 2015 at 14:06

Which SPL are you using to build this with?

I used the package for the 401C Discovery as my starting point.

You'd want to make sure that the HSE_VALUE defined for the project, that it is 8 MHz, not 25 MHz. You also want to make sure the PLL settings reflect this, and the lower speed of the 401 parts.

I'm also not sure why you need to #include everything individually. If you use ST's project templates these will be brought in via the stm32f4xx_conf.h file. Check you have USE_STDPERIPH_DRIVER defined.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dman
Associate II
Posted on November 21, 2015 at 21:43

Hi,

The SPL is V1.6.1 - October 2015.

I've got these defines in my Keil project setup: USE_STDPERIPH_DRIVER,STM32F401xx,HSI_VALUE=80000000,HSE_VALUE=8000000

The only templates I am aware off are the ones generated by STMCubeMX and it automatically includes all HAL libraries. I've generated a demo project, removed all HAL libraries and included only the ones I've needed from the SPL. Probably not the best way to go about it, I agree.

Thanks

dman
Associate II
Posted on November 21, 2015 at 22:06

Got it working. I've set my defines to USE_STDPERIPH_DRIVER,STM32F401xx,HSE_VALUE=8000000,HSI_VALUE=16000000 and Xtal to 16.0

Seems to be working.

Thanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.