STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt Timer

Posted on December 06, 2015 at 01:11The original post was too long to process during our migration. Please click on the attachment to read the original post.

kelly by Associate
  • 1740 Views
  • 3 replies
  • 0 kudos

Warmin up resistor with PID controller

Posted on December 05, 2015 at 14:30How you can warm up resistor. I have the task of warming up resistor to set the temperature with PID controller via usart. Please help ! microcontoller: STM32F411RE

bartes19 by Associate
  • 1422 Views
  • 3 replies
  • 0 kudos

STM32CubeMX USB HS Mass Storage Class code 10

Posted on June 17, 2015 at 09:34 Hi, I have an STM3240G-EVAL board and I try to configure the USB-HS with the SD-Card. I have seleccted: - USB-OTG-HS: External Phy - Device_Only - SDIO: Mode - SD 1 bit - USB_DEVICE: C...

stock23 by Associate II
  • 1954 Views
  • 3 replies
  • 0 kudos

Weird Measured Power Curve for the Stm32f407 Discovery Kit

Posted on December 04, 2015 at 19:22Hi, In a goal of a personal project, i am trying to profile energy consumption of an ARM MCU board, so i take the ''stm32F407 discovery kit'' as an experiment example.In my power measurement experiment i always ge...

nadir by Associate
  • 750 Views
  • 1 replies
  • 0 kudos

Problems with input capture on Nucleo152RE

Posted on December 04, 2015 at 16:46I am working on a Nucleo152RE using EmBitz. The code generates a PWM signal (200Hz 50% duty-cycle) on PB8 (TIM4 channel 3) (It works, I tested with an oscilloscope), then gives this signal as input to PC6 (TIM3 ch...

stm32f427 flash dual bank IAP, random hard faults

Posted on December 04, 2015 at 15:06Hello,I am working on in-application programming of STM32F427, 1MB flash. I have set the DB1M bit in the flash option control register, so the flash memory is organized as two banks of 512 Kbytes each. I am trying...

RTC on STM32F746G-DISCO Ploblem

Posted on December 05, 2015 at 09:10Hi I'm trying to get the RTC work on STM32F746G-DISCO Board. The problem I'm facing is the calendar counter except SubSeconds stop counting after calling the function HAL_RTC_GetTime() since the first time. I've t...

gtopba by Associate II
  • 689 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.