2015-12-06 7:02 PM
For the Chip STM32L151RBH6, we have only 1 bank, EEPROM writting halt the MCU. I make a test program to repeatedly write EEPROM. Use the code like below to write EEPROM:
*(__IO uint32_t *)addr = data; 100 times repeated write consumed 673ms: 6.72ms once. 50 times repeated write consumed 336ms:6.72ms once The Reference Manual addressed: ''This function can be executed from any memory. If it is from the same bank the program is stalled for one Tprog.'' So I tried to implemente the write from Ram function. The result didn't change great. 1. 50 times consumed 324ms, 6.47ms 2. 100 times 663ms, 6.63msWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.