STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuring SDADC and ADC Repeat Triggering With DMA

Posted on January 16, 2016 at 07:06I am triggering ADC1 from TIM4->CCR4 and SDADC1 from TIM4->CCR1. ADC1 is configured for regular conversions and no injected conversions. SDADC1 is configured for injected conversions and no regular conversions. For...

spflanze by Associate II
  • 1479 Views
  • 2 replies
  • 0 kudos

STM32Cube Bug - HAL_RTCEx_SetWakeUpTimer_IT

Posted on February 12, 2016 at 22:42 I'm using the HAL libraries to set up and control the RTC features of an STM32F3 device. The RTC is based on LSE, and is running fine. However, when enabling the wakeup timer, no interrupt was ever generated ...

erik2399 by Associate
  • 956 Views
  • 0 replies
  • 0 kudos

How to generate PWM output using timers on PB0 and PB1

Posted on January 21, 2016 at 15:58 Hi all, I have the stm32F429 micro and I need to generate 2 PWM Output (see below) using pin PB0 and PB1. I tried with toggle mode and TM3 on ch3 and 4, but the duty is 50/50 and is not good. There is a phase...

0690X00000605KoQAI.png
marco2 by Associate III
  • 5948 Views
  • 11 replies
  • 0 kudos

Stm32f4cube 1.11.0 have a bug

Posted on February 11, 2016 at 07:05when I enable USB host and FatFs , Init function in Main created . But it dose not workint main(void){  /* USER CODE BEGIN 1 */  /* USER CODE END 1 */  /* MCU Configuration-----------------------------------------...

usb hangs: stm32f4

Posted on January 31, 2014 at 17:31Hi,I am implementing a CDC USB device using the STM32f4 and STM USB libraries.What I am finding is that after sending a number of multi-byte packets from the PC > STM32 the OUT pipe effectively hangs and I receive ...

mark2399 by Associate II
  • 1884 Views
  • 3 replies
  • 0 kudos

8Gb SDcard with SPI ?

Posted on February 12, 2016 at 00:40Guys, Can I use 8Gb with FATFS and SPI ? Or I need to use 1Gb ? Thanks

EEPROM writing operation optimization ?

Posted on February 12, 2016 at 15:32Hi, I am using STM32L051, I need to write a big amount of data (200 bytes) in the memory . Today this operation takes about 1,4s . But it is too slow . In the RM0377(page 71), there should be a means to write a...

tingting by Associate II
  • 859 Views
  • 0 replies
  • 0 kudos

NUCLEO-F401RE Motor Controller

Posted on February 11, 2016 at 19:37I'm working on a little demo board to evaluate responses of different mosfets and one of the easiest ways to do this is to construct a motor controller. Can the NUCLEO-F401RE be used like the arduino uno in the li...

STM32F1 and STM32F4 external oscillator circuit shorted

Posted on February 11, 2016 at 20:14Hello,I am facing quite strange issue when some of my boards are suffering very rarely from burned path in the MCU for external oscillator input.It happen with STM32F1 and also STM32F4 in the way, that I can measu...

zexx86 by Associate II
  • 1798 Views
  • 2 replies
  • 0 kudos

STM32 no complementary PWM for channel 4

Posted on February 12, 2016 at 13:52Hello there, I have noticed a while a go, that STM32 feature nice timers 1 and 8, which can be used for effective motor controll thanks to complementary outputs and deadtime mechanism. However, for some reason non...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.