STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX and BUG in UART_DMATransmitCplt

Posted on November 02, 2015 at 12:53STM32CubeMX V4.11STM32Cube FW_F4 V1.9.0/**  ******************************************************************************  * @file    stm32f4xx_hal_uart.c  * @author  MCD Application Team  * @version V1.4.1  * @d...

When to use DMA on USART

Posted on June 09, 2016 at 11:29Hi,I'm fairly new to micros with DMA and am wondering when to use the DMA to create a cyclic buffer.Background...I'm looking to update some working but un-maintainable drivers, eventually I'll be sorting I2C, ADC, SPI...

PolarSSL

Posted on June 07, 2016 at 16:48Hello, is the Polar SSL (mbed TLS) Stack running without RTOS ? Thanks in advance Michael

STM32F103 USART - PC receives wrong data

Posted on June 08, 2016 at 11:45 Hi guys, I've implemented the code to send data from STM32f103 to PC with USART interface, but the data that I receive are wrong. This is the code that I've implemented : void RCC_Configuration(...

0690X0000060395QAA.jpg
verdano by Associate II
  • 7407 Views
  • 16 replies
  • 0 kudos

FW repo source files incomplete?

Posted on June 08, 2016 at 08:08I have been trying, with limited success, to create a project in CubeMX and then import the example application files from LwIP HTTP server app so I can start to find a solution for my specific tasks.  In the process ...

SIM800 with stm32f334

Posted on June 09, 2016 at 02:21Hi all;I am trying to send sms using sim800l module with stm32f334&sharpinclude ''mbed.h''&sharpinclude <string>Serial pc(SERIAL_TX, SERIAL_RX); // pc comunicationSerial SIM900(PA_9, PA_10);   //tx, rx SIM 900string r...

SDIO IRQ Being Blocked?

Posted on June 08, 2016 at 18:41I'm having issues with my SDIO Data End interrupt.It's acking like OCCASIONALLY the SDIO interupt it being blocked by the SDIO_DMA IRQ. The SDIO has a higer priority (lower number) interrupt than the DMA.I'm using stm...

Newbie Q: Getting just GPIO to work with STM32CubeF0

Posted on June 07, 2016 at 06:00I am just getting started on STM32 micro-code development for a custom board built around the STM32F072. I downloaded the CubeF0 and was able to build a few sample projects.I now want to extract just the GPIO parts (s...

gaurav2 by Associate II
  • 1654 Views
  • 3 replies
  • 0 kudos

stm32CubeMX stm32f407 discovery printf doesn't work

Posted on December 15, 2015 at 10:46Hi all, trying to retarget printf on stm32f407 discovery with cubemx generated code isn't working. Inside main.c i've put:/**   * @brief  Retargets the C library printf function to the USART.   * @param  None   * ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.