STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About HAL_UART_Receive_IT arguments

Posted on August 18, 2016 at 18:33 One slip of my finger and my post was gone. I hope this is not a duplicate post. I am receiving serial data one byte at a time. For that I need an one byte array, I think. Does it have to be an array? O...

LMI2 by Lead
  • 1206 Views
  • 1 replies
  • 0 kudos

Key matrix example code

Posted on August 18, 2016 at 17:52Hello,I need 4x4 key matrix IAR example C source code for STM32F series.It would be very helpful for me if you can give me.Thanks in advance! #key-matrix #keypcad

w21685 by Associate II
  • 1368 Views
  • 1 replies
  • 0 kudos

SDRAM connections on FMC

Posted on August 18, 2016 at 17:55Hi,Hoping for some feedback from ST or others who have tested/used this configuration...The datasheet for the STM32F745xx (also the 746xx) contains Table 11. This shows the FMC pin definition, and lists the followin...

STM32F405 corrupt i2c transactions

Posted on August 17, 2016 at 14:06Hi!I have been writing my own I2C driver to play well with the RTOS and I have been using a I2C analyser to help me out. After a lot of frustration I have gotten most of it working but what I have discovered is that...

0690X00000603BHQAY.jpg
tobias by Associate II
  • 1899 Views
  • 2 replies
  • 0 kudos

Combining Firmware Examples

Posted on August 16, 2016 at 02:09I have the example projects compiling, loading, and running from the F4xx firmware repository and it works perfectly.  I am using the lwip from project > application and wish to add control over a PWM output.  I too...

Fail to launch STLINK debugger

Posted on August 16, 2016 at 14:40Hi.Its been so long since my last project with STM32, and I have created a new C project with SW4STM32 for my stm32vl discovery board and when I try to run the debugger, I get the following error. Error in final lau...

mbmail4 by Associate II
  • 1196 Views
  • 4 replies
  • 0 kudos

STM32F4-Discovery 5V pwm

Posted on August 17, 2016 at 20:06Hello, I currently have a 3.3V PWM on TIM3_Channel2.Can the output be changed to a 5V logic?Sel

selmesal by Associate II
  • 721 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.