STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Conneect to NTP server

Posted on September 14, 2016 at 12:35Hello, I want to use Ethernet peripheral to connect to NTP server. It's my first time to use this peripheral so can I just use this driver to connect to it or something still missing? and are there ready APIs to ...

STM32L031G6 flashing problem

Posted on September 14, 2016 at 09:26Hi, I need to flash my code into STM32L031G6 chip using an external debugger, but i got the following error: ERROR: Timeout while checking target RAM, RAMCode did not respond in time  Failed to prepare for progra...

duybienle by Associate II
  • 3349 Views
  • 1 replies
  • 0 kudos

HAL UART Receive with Interrupt issue

Posted on September 13, 2016 at 22:12Hello everyone i'm a beginner, i have implemented uart receive of variable number of characters successfully using IRQ and RXCmpltCallback , what i did is i have received each character one by one and then insert...

mushfiq by Associate II
  • 1442 Views
  • 2 replies
  • 0 kudos

stm32f4 UART HAL losing bytes

Posted on September 13, 2016 at 11:20Hi All,I'm working on stm32f411 borad with hal library.I'm using the UART without knowing the exact size I suppose to get so I'm using HAL_UART_Receive_IT to get the first byte of the data and afterwards I use HA...

123456 by Associate II
  • 1946 Views
  • 3 replies
  • 0 kudos

nucleo-F746ZG I2S example

Posted on September 13, 2016 at 20:26Hi all,I'm trying to use the NUCLEO-STM32F476ZG board as an i2s-connected host platform for some prototype C++ DSP code.We are having trouble running the i2s example in STM32Cube_FW_F7_V1.4.0 :Projects/STM32F746Z...

STM32F746G USB Device MSC with FatFs_uSD

Posted on September 14, 2016 at 03:11Hardware used:Nucelo Board -- STMF746ZG - Nucleo 144I have been trying to adapt the USBD_MSC code written for the STM32F746G Discovery Board for the Nucleo 144. Running the USBD_MSC example works great, and I can...

jjohnson by Associate
  • 822 Views
  • 0 replies
  • 0 kudos

Large display project

Posted on September 10, 2016 at 18:51I am new to the STM32 platform.  I have an embedded project I have been attempting to build for quite some time that needs a large display space.  The processing of the project is not high, there is just lots of ...

ray23 by Associate II
  • 2995 Views
  • 4 replies
  • 0 kudos

Looking for GCC based CDC code for F107 that actually works

Posted on May 19, 2016 at 17:42Folks, I've spent almost two weeks trying to get a virtual com port (VCP) working on an F107 with FreeRTOS and am getting problems whichever thing I try. I started with an old version of FreeRTOS with old libraries and...

DiBosco by Senior II
  • 2807 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.