STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFaultException in RAM-Test

Posted on September 22, 2016 at 14:55The RAM-test procedure STL_FullRamMarchC(void) of the IEC 60335 SelfTest library ends with a HardFaultException. Debugging the function Shows that this happens after Step 6.  The return address seems to be lost. ...

Nucleo f429zi after st-link removal

Posted on August 29, 2016 at 11:04Hello,I have a following problem, I have a Nucleo f429zi board and after ST-link removal I am unable to run code on it. I've chcecked the solder bridges, I'm using SWO - the debbuging seems to be fine, the cpu is st...

SimonP by Associate II
  • 1269 Views
  • 1 replies
  • 0 kudos

stm32f107 - SPI ''reinit'' not working

Posted on February 14, 2016 at 21:24 Hi, i write bootloader with sdcard upgrade option. During first bootloader start (after power on, or MCU programming using stm-vldiscovery programmer) everything works well. When I restart MCU using N...

STM32F0 Comparator Output issue

Posted on September 02, 2016 at 19:53I am unable to get any output from the COMP1 comparator on an STM32F072RB on any pin other than PA0. The datasheet ''STM32F072x8 STM32F072xB'' states on pg 41 that COMP1_OUT should be available on pins PA0 PA6 an...

STM32F746G_DISCO USB and UART Issue

Posted on September 01, 2016 at 05:34Hello, We bought 10 of these boards and want to run USB host and log screen outputs through UART6 to Hyperterminal. When we run the USB host example, things work fine. When we run UART_com_IT standalone, things w...

david2399 by Associate II
  • 1175 Views
  • 1 replies
  • 0 kudos

BSP_AUDIO_OUT_Play function stops program execution

Posted on September 18, 2016 at 17:47Hi. The function BSP_AUDIO_OUT_Play stops the program flow completely even before the return value can be read. The audio buffer is output as a never ending loop. The BSP_AUDIO_OUT_Init worked well with no error ...

STM32F101 current draw in Stop mode

Posted on September 21, 2016 at 17:42I discovered ~450uA additional current draw coming from the STM32F101 in Stop mode.  This condition occurs when an external pin interrupt from a peripheral goes active during Stop mode even though the NVIC is dis...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.