STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

An ''old-fashioned'' question about SCSI Bus...

Posted on October 14, 2015 at 06:44Hello There,Yesterday while I was reading through the STM32 USB-FS-Device development kit for the first time (UM0424), I was really surprised that the SCSI Protocol Implementation is part of this software library. ...

Zaher by Senior II
  • 1653 Views
  • 3 replies
  • 0 kudos

SD card writing in DMA mode.

Posted on September 19, 2016 at 09:55  The original post was too long to process during our migration. Please click on the attachment to read the original post.

rajesh23 by Associate II
  • 4995 Views
  • 6 replies
  • 0 kudos

stm32f429 external rtc

Posted on September 21, 2016 at 15:30Hi,I am using stm32f429ZIT6 mcu for my own board. I want to create 1 second interrupt with external 32.768Khz rtc but it doesn't work. My Systemclock config and rtc init functions are below:void SystemClock_Confi...

er3481 by Senior
  • 1822 Views
  • 4 replies
  • 0 kudos

16bit SDADC SIGMA DELTA STM32F373 doesn't work

Posted on September 06, 2016 at 20:06Hallo,I use the Mikroe compiler and don't get the SDADC for work :(Is there a step by step manual, which values I have to use in which order?!Maybe1. enable SDADC2. Initlialice3. calibrateor maybe1.Init2. enable?...

sven by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

32F7 JTAG and openocd

Posted on September 19, 2016 at 19:01opened problem with stm32F7 ?Dear All,I am using JTAG openocd to program the stm32f7 flash. I am facing to a strange behaviour. I can program the cpu flash but I have to reduce the clock of the JTAG to 100KHz. Ex...

Triggering SDADC (stm32f373) from RTC (LSE)

Posted on September 22, 2016 at 15:19Hello, I have a project based on stm32f373, I'd like to trigger sdadc conversion with RTC synchronyzed frequency, are there any solutions to do this without external routing MCO output(LSE) -> Timer Input -> Trig...

mailbox by Associate II
  • 1104 Views
  • 1 replies
  • 0 kudos

Change static library target device in SW4STM32

Posted on September 11, 2016 at 10:16Hi,I use the SW4STM32 IDE and would like to create a generic static library.When I go to New Project tab and select static library in ''Project type'', I can create ''Ac6 STM32 MCU GCC'' or ''Cross GCC'' project....

heifetsg by Associate II
  • 1247 Views
  • 1 replies
  • 0 kudos

Resolved! SPI NSS do not change. HAL libraries

Posted on September 22, 2016 at 12:51Hi all; I am trying to comunicate with an external flash memory with my STM32F429. I can see my signals in the oscilloscope . I see how my microcontroler starts the clock and write to the bus but the NSS signal d...

jzotes by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos

STM32F401 Apple-1 Replica Emulator

Posted on September 22, 2016 at 13:24Hello to All, recently I coded an emulator of an old Apple-1 inside a STM32F401 Discovery board. It is capable to generate a PAL/NTSC composite video signal, it's interfaced to an old Macintosh 128K keyboard thro...

0690X00000603CJQAY.jpg 0690X00000603COQAY.jpg 0690X000006039GQAQ.jpg 0690X0000060367QAA.jpg
Digimorf by Associate III
  • 1403 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.