STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_RxCpltCallback stops reading on 0x00

Posted on November 20, 2016 at 00:32 Hallo, I try to read binary data from PC to STM32 F Data are framed in following format. DLE STX DATA DLE ETX (0x10 0x02 DATA 0x10 0x03). My goal is to read DATA bytes. I'm usingHAL_UART_RxCp...

vancom by Associate
  • 846 Views
  • 0 replies
  • 0 kudos

Workaround interfacing STM32F429 FMC with a TFT

Posted on November 18, 2016 at 16:39Hello,I am working with a smart TFT that supports the 8080 parallel interface on a custom board but the design omitted connecting the RD, RS, CS, WD to the appropriate NEx, NOE, NWE, Ax pins. Instead these 4 contr...

Disable RX TX Callbacks - Uart DMA stop

Posted on December 17, 2015 at 07:21 Hello there, I am using uart tx and rx with dma. It works, but each time I stop the DMA using: /** * @brief Stops the DMA Transfer. * @param huart: pointer to a UART_HandleTypeDef structure tha...

NUCLEO L152RE Hardware version

Posted on October 27, 2016 at 14:06Hi!I have three Nucleo-L152RE Board with this features:- Board 1 and Board 2:  STM32L152RET6GH23W, Hardware version: MB1136 C-02- Board 3: STM32L152RET6GH245, Hardware version: MB1136 C-03I made a program that use ...

Microcontroller programming issue after connecting VBUS

Posted on November 04, 2016 at 14:19HeyI am using STM32F429VIT6. I have ported the USB_CDC program from the example and was working fine with the Evaluation board. I have changed the program to work with the MCU and ported the program. I havent enab...

dixon by Associate II
  • 1236 Views
  • 1 replies
  • 0 kudos

STM32F7 HS-USB ULPI PHY options from Microchip

Posted on November 12, 2016 at 20:34Hello, you may remember STM32F2 and F4 had troubles with some HS-USB ULPI transceivers from Microchip. I wonder if these issues exist with STM32F7 too ? I'm especially interested in USB3317 and USB3343. I've notic...

STM32F427 FMC connected SDRAM

Posted on November 17, 2016 at 12:16Hi guys, we have a IS42/45S16100H device connected to STM32 FMC bus ( BANK2 ). If we run the application from internal SRAM everything is fine. Unfortunately, if we use the SDRAM as heap, we have trouble. Someti...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.