STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I can't configure SPI1 on STM32F103C8

Posted on November 25, 2016 at 07:04Hi!I have STM32F103C8 and want to configure SPI1!I wrote the program//spi1_mosi-pa7,spi1_miso-pa6,spi1_sck-pa5,spi1_nss-pa4#include ''stm32f10x.h''int main() { RCC->APB2ENR=RCC_APB2ENR_IOPAEN; RCC->APB2ENR|=RCC_AP...

STM32F103 Usart data receive problem

Posted on November 25, 2016 at 07:32 Hello all, Directly, I want to talk about a problem I have encountered.I am working on 2 types of microcontroller and I use stm32f103 model to get data from the other one via rs4 So, For transmi...

0690X0000060MnbQAE.gif 0690X0000060MncQAE.gif 0690X0000060MndQAE.gif
pm_brk_pm by Associate II
  • 1754 Views
  • 1 replies
  • 0 kudos

STM32F746VGT6 Pinout

Posted on November 24, 2016 at 23:38I'm trying to build a custom PCB to control an graphic RGB 24 Bit TFT LCD.It seems I cannot find any were in the datasheet pins for LCD_R0 and LCD_B1 on an LQFP100 package.Can anyone help me, or explain why are th...

luchiann by Associate
  • 1207 Views
  • 1 replies
  • 0 kudos

STM32 EEPROM AUTO ERASE!!

Posted on November 20, 2016 at 14:21Hello,I am posting on any thread 1st time so don't know if i m writing it right.I am using STM32f103V8T6 and reserved 2kb for storing my settings in location start address 0x0800F000 and end address 0x800 reserved...

adil by Associate II
  • 3642 Views
  • 7 replies
  • 0 kudos

Problemwith SWD debugging on STM32L011D4P6

Posted on November 22, 2016 at 23:09Hi,We are bringing up a new design using this CPU. Aside from other issues, we have an inconsistency between different boards when trying to program using SWD. On one working board, the SWD clock (pin 2 on the 10 ...

Where can I find libraries???

Posted on November 23, 2016 at 16:48Hi, I am new with the ST microcontroller and I was looking for some basic libraries. I am using a STM32F373CC and I want to use the SPI, ADC and DAC on the microcontroller... I have used the STM32 cube software to...

How to read Device ID Register in IDE

Posted on November 14, 2016 at 22:47I am using an STM32VLDISCOVERY with an accelerometer which is connected using SPI. I am trying to determine whether or not I have it connected to the STM correctly so I am trying to read its Device ID through the ...

Trying to make a USB HID mouse from cube mx

Posted on November 21, 2016 at 07:04 i have tryed to make working an usb hid mouse program (simulating mouse move) from cubemx: usb_otg_fs folowing youtube stm sample: https://www.youtube.com/watch?v=XRocqTfUxbo my platform is STM32F746DI...

0690X0000060MoOQAU.gif
lrou13 by Associate II
  • 1734 Views
  • 3 replies
  • 0 kudos

L4 LL drivers

Posted on October 12, 2016 at 19:06I'm confused about the development strategy.  Ideally, the Hal drivers should be layered on top of the LL drivers.  However, when I look at the code for say  gpio or spi, the Hal drivers duplicate the LL functional...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.