Dimmer 4ch
Posted on November 12, 2016 at 15:57I would like to drive 4ch dimmer triac with input sync zero crossing. I want to use the timer device of stm32. How I do initialize the timer for drive 4 ch triac with input trigger sync zero crossing?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on November 12, 2016 at 15:57I would like to drive 4ch dimmer triac with input sync zero crossing. I want to use the timer device of stm32. How I do initialize the timer for drive 4 ch triac with input trigger sync zero crossing?
Posted on November 30, 2016 at 17:27Hi,I am currently working with STM32CubeMX V4.17.0 and the firmware package for family STM32F7 V 1.5.1 I need to set up my cube project so that I have access to the HAL routines for The CRYPTO and HASH modules, bu...
Posted on August 04, 2016 at 19:11I am starting on a new project and though I would give STM32CubeMX a try.I have entered my custom configuration in STM32CubeMX, but there is no code generation option for the IDE I am using (Rowley's CrossStudio). ...
Posted on November 25, 2016 at 03:45Dear Sir,Take a look the global constant contained in comdef.h.typedef unsigned char boolean; /* Boolean value type. */typedef unsigned int uint32; /* Unsigned 32 bit value */typedef unsi...
Posted on November 29, 2016 at 20:25Hello, I am new to embedded electronics MCU's.However, I am hoping to start working on a prototype for a tactile physical control surface that incorporates a number of simple analogue controls (see below) that is ...
Posted on November 28, 2016 at 13:24 Hello, Im using NI Can with labview application that shows recieved messages. the cortex is connected to transciever. Both NI and the transciever are terminated correctly. when im starting to trans...
Posted on November 25, 2016 at 19:43Fails to compile: ..\..\..\..\..\..\..\..\Drivers\CMSIS\Device\ST\STM32L4xx\Include/stm32l476xx.h:185:30: fatal error: system_stm32l4xx.h: No such file or directory compilation terminated. I've seen this before - ...
Posted on October 09, 2016 at 06:06Hi, I am looking to have sd card interfaced with SPI using FATFS library, I have spent a lot of time trying to figure out how to do it but without any success. Could anyone help me with that? Thanks.
Posted on November 30, 2016 at 07:02 I am sending the correct command and I can see it on the scope.However, I don't get 0x01 response(I keep getting 0xff) from SDcard(SDHC)(SanDisk Ultra 40MB/s ...16GB) I am using the following code: ui...
Posted on November 16, 2016 at 10:08The original post was too long to process during our migration. Please click on the attachment to read the original post.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.