2016-11-29 10:02 PM
I am sending the correct command and I can see it on the scope.However, I don't get 0x01 response(I keep getting 0xff) from SDcard(SDHC)(SanDisk Ultra 40MB/s ...16GB) I am using the following code:
uint8_t cmd0[6]={0x40,0x00,0x00,0x00,0x00,0x95};
uint8_t dumb=0xff;
FATFS_CS_HIGH;
for (int i = 0; i < 10; i++) {
HAL_SPI_Transmit(&hspi1, &dumb, 1, 10);
while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY);
}
FATFS_CS_LOW;
HAL_SPI_Transmit(&hspi1, cmd0, 6, 10);
while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY);
for (int i = 0; i < 10; i++) {
HAL_SPI_Transmit(&hspi1, &dumb, 1, 10);
while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY);
}
HAL_SPI_Receive(&hspi1, &c, 1, 10);// I keep getting 0xff
2016-11-30 7:01 AM
Hello,
Your code is not clear. Please, reformulate it using ''Format code block'' to get help.You can refer to the working SPI examples with STM32CubeF3, this may help you in SPI initialization and configuration.RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.