STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fixing my STemWin LCDConf - what is this effect called?

Posted on January 27, 2017 at 15:11Looking to straighten out my LCDConf but I don't know where to begin. What is it called when a screen does this? Please see the attached image. If i knew what it was called when a screen does this, I could at least...

Training/Tutorial USB-UART for STM32F4?

Posted on January 26, 2017 at 18:24Hello there,Im working with nucleo144F429ZI and i want to implement a USB CDC VCP Device for Tx/Rx-Data over the USER USB.I already managed to get the CubeMX generated Sourcecode to run on the board... Sometimes.Wi...

[BUG] STM32CubeF4 HAL_GPIO_DeInit()

Posted on January 27, 2017 at 17:13Hi,just reporting another issue with the HAL lib 1.14 for STM32F4When you first init a GPIO as EXTI and then deinit it with the HAL_GPIO_DeInit() function it will not mask the pin int source.. although it is mentio...

Connect bits streams at 13Mhz to GPIOs

Posted on January 23, 2017 at 23:54Hello,I have a board which have 8 x bit streams. Each bit stream has its own associated bit clock. So I have: 8 x 2pins (one for the bit stream, one for its associated bit clock). Each bit clock is at 13mhz.I would...

michcfr by Associate II
  • 7232 Views
  • 17 replies
  • 0 kudos

STM32CubeMX - Bug - IAR Project Generator

Posted on November 21, 2016 at 14:09Path of HAL driver is incorrect in the project generated by CubeMX when using following config:A none default toolchain folder + Add library files as references. Then in the generated project IAR can't find HAL dr...

0690X00000604vvQAA.png 0690X00000604wcQAA.png 0690X00000604q2QAA.png
MasterPhi by Associate II
  • 1345 Views
  • 2 replies
  • 0 kudos

Resolved! NucleoF303K8 NVIC_Init() hang

Posted on January 27, 2017 at 13:40 Hi, everyone! I am working on a NucleoF303K8. I am using the standard periph library. I am trying to use USART interrupt in my project, but being held by a problem. When I NVIC_Init() the USART interrupts, it h...

Li JW by Associate II
  • 2111 Views
  • 3 replies
  • 0 kudos

Hard fault when accessing STM32L0 calibration values

Posted on January 27, 2017 at 11:39 Hi, When accessing some calibration registers, I get a hard fault. It might be due to unaligned access. Is the ' stm32l0xx_ll_adc.h,V1.7.0' correct? The 'VREFINT_CAL_ADDR' works correctly. 'TEMPSE...

STM32F427 CAN FD

Posted on August 26, 2016 at 10:31I am curently using the STM32F407 and F427 MicroControllers. Can anyone advise if they are CAN FD compatible or if this is a software layer etc. Any information would be helpful. Rgds John W

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.