2016-08-26 1:31 AM
I am curently using the STM32F407 and F427 MicroControllers.
Can anyone advise if they are CAN FD compatible or if this is a software layer etc. Any information would be helpful. Rgds John W2016-08-26 2:54 AM
Pretty sure it is an accelerated signalling mode, and not a software layer tweak, so no I don't think this is supported by the bxCAN controller used by ST.
2016-08-26 3:20 AM
Thanks Clive.
I think CAN FD has a 8 byte to 64 byte data flexability. Maybe ST support can advise on availablity. Once again thanks for help ... and in the past. KR John W2016-08-30 1:37 AM
for can-fd the can-controller within the silicon has to be modified. as far as i know there a some vhdl implementations for fpga's.
or you check the vendors for an external can-controler with spi interface and can-fd support.2017-01-27 3:22 AM
Hi
White.John
,The CAN FD is not supported on our current products, but it will be available on STM32H7:
https://community.st.com/0D50X00009XkihHSAR
-Nesrine-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.