STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA Transfer with Data Size larger than 65535

Posted on March 13, 2017 at 16:13Board: STM32F767 Nucleo-144.I use DMA to transfer results sampling from ADC at 1MHz to SRAM, but the data size is quite large which is 240k samples (480kbytes). However, a single DMA transfer (calling HAL_ADC_Start_D...

The LL drivers for F4

Posted on March 03, 2017 at 14:03The documentation here (http://www.st.com/content/ccc/resource/technical/document/user_manual/2f/71/ba/b8/75/54/47/cf/DM00105879.pdf/files/DM00105879.pdf/jcr:content/translations/en.DM00105879.pdf) states that the F4...

achin by Associate II
  • 2920 Views
  • 5 replies
  • 0 kudos

Problems leaving ADC_Conv_CpltCallback function

Posted on March 10, 2017 at 13:00Hallo together,I am using a STM32Nucleo-Board with the STM32F401RE-Controller in combination with the PLC expansion board.I have used the Cube MX tool to generate the initialization for the peripherie constisting of ...

Update of DocID029289 Rev1

Posted on March 13, 2017 at 18:12Hi,I am using the Steval-3DP001V1 with the DocID029289 Rev1 does anyone know if there is an update of this doc because with the code on gitHub Marlin4ST in Eclispse Luna the path doesn't match with thoses descriped i...

STM32F407 TIM1CC

Posted on March 12, 2017 at 18:33I can't seem to get TIM1's CC channel 1 ISR to fire. FanTimerHandle.Instance =TIM1;  memset(&sConfig, 0, sizeof(sConfig));  /* Initialize TIMx peripheral as follow:       + Period = 0xFFFF       + Prescaler = 0      ...

Sample Point CAN Bootloader?

Posted on February 19, 2017 at 21:38I am currently reading the AppNote AN2606 and AN3154 to use the CAN Bootloader.But in the AppNotes I found no information to the CAN timings.Can someone tell me how the sample point must be adjusted to communicate...

Resolved! Timing-Jitter on gpio output when LCD is active.

Posted on March 08, 2017 at 16:06Hi guys,we have a problem here. We run a Stm32F469BITx at 180 Mhz. There is a lcd display and a realtime process included. The realtime process creates GPIO-Pin-Changes in Mikrosecond intervalls. The problem is that ...

LAN8742A_PHY_ADDRESS wrong address

Posted on March 02, 2017 at 15:02I do have the same issue https://community.st.com/0D50X00009XkgMqSAJ  with the code generated for the stm32F2 device.Additionally some values are not correct, below is the value we should have (based on the demo for ...

Adalgiso by Associate II
  • 2720 Views
  • 5 replies
  • 0 kudos

CubeMX - FatFS - SDIO not working

Posted on July 09, 2014 at 11:09Hello,I'm trying to make working the fatFS thought SDIO-4bits but I have the same problem on 2 different boards (devkit and custom board with STM32F437).All the code is generated by cubeMX (v4.3, firmware 1.3).The MX_...

campbiel by Associate II
  • 4304 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.