STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SW4STM32 + STM3210C-Eval Hello World program

Posted on February 03, 2017 at 21:58I am evaluating an STM32 chip with CAN with respect to the CAN enabled bootloader.I have programmed for years on the TI CCS IDE on ARM4s.  SW4STM32 is a similar IDE.I have SW4STM32 installed.  I have the STM3210C ...

John Osen by Associate II
  • 2898 Views
  • 3 replies
  • 0 kudos

Bug on cmsis_os.h on stmcubemx 4.19.0 ?

Posted on February 22, 2017 at 10:18Hi, i'm using stmcubemx 4.19.0 for my project on stm32f415vgt.But i think it's present a little bug inside cmsis_os.hWhen i create queue, the item size is never 0x04.&sharpdefine osMessageQDef(name, queue_sz, type...

Marco1 by Associate II
  • 1900 Views
  • 6 replies
  • 0 kudos

Resolved! How to setup SW4STM32 to use Rlink

Posted on February 09, 2017 at 23:19I am new to both SW4STM32 and the emulator Rlink.  Rlink works with Ride7; however, there are some .ld tricks I cannot get to in Ride7.How do you setup Rlink to work with SW4STM32?Alternatively, how do you get the...

John Osen by Associate II
  • 2385 Views
  • 4 replies
  • 0 kudos

stm32L073RZ bootloader

Posted on March 22, 2017 at 11:27Hi guys,I'm working on a firmware update on-the air (FOTA) on a L073RZ. I found a project working on L4s, this project uses the L4's bootloader in order to then run the app. This bootloader is in the project's folder...

L476 Problems getting the FMC working with SSD1963

Posted on March 09, 2017 at 00:15We are having problems trying to make a 320x240 LCD Color Display working on the L476 FMC Peripheral.  The LCD uses the SSD1963 chipset.  We have hooked the SSD1963 up to the FMC like an 8080 SRAM device using the pa...

Initialize TIM1 Break Input using STM32CubeMX

Posted on March 23, 2017 at 09:54Hello, I'm using STM32F4Discovery for single phase inverter project.I need to use the break input of TIM1 for protection of my MOSFET driver and the MOSFET itself. After taking a few days trying to initialize break i...

0690X00000603iFQAQ.jpg
ade by Associate II
  • 879 Views
  • 0 replies
  • 0 kudos

Can i use NVIC_ SetVectorTable in STM32F722RE MCU ?

Posted on March 23, 2017 at 08:08Dear Due to i need to modify vector table address, can i use 'NVIC_ SetVectorTable' this function? or i need to modify &sharpdefine VECT_TAB_OFFSET  in system_stm32f7xx.c   I always get link error and can't find whci...

Problem With USART

Posted on March 22, 2017 at 11:55Hi,I am using 3 USART in my code, But I faced a one ridiculous problem with them.USART2 configured on interrupt and working fine I have No problem with this one. I Initialize the USART3(POL) first and send some data ...

bhavesh by Associate II
  • 2684 Views
  • 5 replies
  • 0 kudos

powerStep01 configuration guide?

Posted on March 22, 2017 at 19:46I'm having trouble getting a powerStep01 configured to run in step clock mode on top of a Nucleo F411RE. Mostly configured as required, but as soon as I try to enable it (hardstop) it throws an OCD and drops out of s...

estie by Associate II
  • 1105 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.