STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f103vbt6 Interrupt Numbers ?.

Posted on July 20, 2017 at 00:15Evaluating the above processor using gcc toolchain and openocd and J-Link. Not using cmsis (various reasons) and writing all the low level hal and header files, as a way to become more familiar with the processor. Alr...

STM32F7 MPU performance impact?

Posted on July 21, 2017 at 23:36Greetings,After reading http://www.keil.com/support/docs/3777.htm it seems like a good idea to change the SDRAM attributes via the MPU.  Can anyone comment on the performance impact of enabling the MPU (it's not curre...

STM32F429 LTDC @ 1280x720 resolution

Posted on May 22, 2017 at 16:17Hello everyone,I already successfully used the LTDC to create a VGA Signal with a Resolution of 800x480 Pixel with 16bitcolour with decent performance. All configuration was done with CubeMX for the LTDC.AN4861 claims ...

Cube F4 V1.16.0 DMA on SD card broken?

Posted on July 07, 2017 at 02:12I'm using Cube generator app V4.21.0 and F4 FW V1.16.0 on a 429II.If I enable DMA transfers for the SD card, it hangs in the SD driver and won't even allow the card to be mounted.Rolling back to older versions of stm3...

Problem in SPI transmission of stm32f072cb

Posted on July 21, 2017 at 16:34Hi guys,I am new to stm32 controller and i am facing a problem in receiving part of spi which is not working can you please explain to me the specific part of the code need to change i am using spi in bidirectional mo...

Why is priority HAL_DELAY compared to button?

Posted on July 20, 2017 at 15:38Hi,i've a little problem with stm32L0.I want change state with button B1, but HAL_DELAY is priority of button. the mian is:uint8_t stato; stato = 0;while (1) {switch(stato) { case 0: HAL_GPIO_WritePin(LD2_GPIO_Port, L...

Lex Trc by Associate II
  • 1878 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.