2017-07-21 2:36 PM
Greetings,
After reading
http://www.keil.com/support/docs/3777.htm
it seems like a good idea to change the SDRAM attributes via the MPU. Can anyone comment on the performance impact of enabling the MPU (it's not currently enabled in our application)?Thanks,
Dave
2017-07-21 2:52 PM
My take away is that it's better to remap the memory. Uncached SDRAM is surely not very desirable.
I know you can fault an M3/M4 if you access a 64-bit (int or double) using LDRD/STRD that is unaligned, haven't tried the M7, and the M0 is a bigger headache like the old ARM7/ARM9 parts
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.