STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

disable read/write protection on STM32L451xx

Posted on August 18, 2017 at 04:30Hi,I've got problem with migrating from stm32l476xx to stm32l451, when using l476, writing to internal flash was never been a problem. But in L451, I've failed everytime I write to the internal flash.I've notice dif...

USART stuck condition, waiting on TC? CTS? STM32F411

Posted on August 18, 2017 at 01:13So, I have a system here that I recently observed a non-reproducible lockup in, so I rushed over and attached a debugger to the running target to see where the problem was.I saw that the UART driver code (at an SDK ...

apullin by Associate II
  • 1153 Views
  • 1 replies
  • 0 kudos

Resolved! RCC_CFGR_MCOXPRE doesn't corrosponde to the manual

Posted on August 17, 2017 at 21:15Hi,has anyone checked in the stm32f4xx.h Lib the RCC_CFGR_MCOxPRE Register?The values mentioned in the RM0090 manual don't fit the stm32f4xx.hstm32f4xx.h:&sharpdefine  RCC_CFGR_MCO1PRE                    ((uint32_t)...

uli stone by Associate II
  • 1634 Views
  • 3 replies
  • 0 kudos

Resolved! bypass config with STDPERIPH_DRIVER

Posted on August 17, 2017 at 13:05hello i use stm32f030f4 and use 10MHz oscillator (BYPASS) and i want achieve to 48mhz in mcu.and i use STDPERIPH_DRIVER and keil v5.what configuration i have to do ?what code i have to add to my project?

Resolved! STM not respecting recommended design guide for HSE crystal

Posted on August 16, 2017 at 18:24I am trying to choose a crystal for the STM32F7. The only problem being is that I cant find a component that respects the recommended values found in the following arm http://www.st.com/content/ccc/resource/technica...

0690X00000607uUQAQ.png
Maz D by Associate II
  • 4031 Views
  • 8 replies
  • 0 kudos

Need Help For CS43L22 On STM32F4 Discovery DK

Posted on August 17, 2017 at 17:071. As I see on stm32f4 discovery DK schematic, CN4(audio jack) only connect to HP/LINE_OUTA and HP/LINE_OUTB ( Pin 14 and 15 of CS43L22). Because of that, I only use OUTPUT_DEVICE_HEADPHONE of CS43L22. Does my thoug...

gcc and PCROP

Posted on August 17, 2017 at 12:59Dear all,the readout protection of the L4, F4 and F7 MCUs is supported with build-tools form Keil and IAR. The 3 application notes, i have read, states that one of these IDEs must be used. Since the newer arm-none-e...

I can't install library to STM32CubeMX

Posted on May 11, 2017 at 22:45Hello,İ just downloaded a library for STM32CubeMX, i just gave library's link below. I just can't install it to Cube. I'm opening the new library manager by clicking install new libraries in help and then clicking the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.