STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART

Posted on July 24, 2017 at 08:08Hi!I am study UART to communicate with PC.My target is use PC like a terminal to input AND out message to STM32.My code is using HAL library.I want to operate code like below.**************************************ch =...

0690X00000607foQAA.png
L C by Associate II
  • 7648 Views
  • 14 replies
  • 0 kudos

32F746GDiscovery UART DMA

Posted on August 29, 2017 at 16:13I am trying to create a module for the 32F746GDiscovery board which will make use of USART6 in a UART configuration that is on the Arduino connector. The time between end of the transmission sent and the reply from ...

Roth.Ian by Associate III
  • 732 Views
  • 0 replies
  • 0 kudos

STM32F746G CubeF7 LwIP demo

Posted on August 28, 2017 at 17:03Hello,I've been trying out the examples from the STM32 CubeF7 projects for the STM32F746G Discovery board, but when I build the LwIP application using the SW4STM32 tools the image is over 393MB and so too large for ...

Using Touch Sensing Controller on STM32L053R8 nucleo64

Posted on April 18, 2016 at 15:18Hi everyone, I'm trying to set up 3 capacitive touch keys using HAL touch sensing controller library but I'm facing some problems. I followed the instructions in AN2869 application note for implementing one sensor us...

Abnormal operation after reset (BOOT0)

Posted on August 29, 2017 at 06:37STM32F103RC Abnormal symptom occurred while using Help request. Resetting without a ground connection to the BOOT0 pin will result in some products not booting. If this problem occurred from the beginning of develop...

Jae Bong by Associate
  • 1127 Views
  • 1 replies
  • 0 kudos

STM32 booloader

Posted on August 28, 2017 at 16:53Hello to all.I'm new user in STM32 and I need to do a CAN bootloader. Only software bootloader! I understand how I can modify the linker script to add the boot region. But my problem is how to jump at the startup in...

Giu S by Associate II
  • 1923 Views
  • 2 replies
  • 0 kudos

STM32F446ZE OTP Lock block programming issue

Posted on August 29, 2017 at 09:37Hello,I use NUCLEO-F446ZE board. And I'm trying to lock OTP block 0 by programming 0x00 at 0x1FFF7A00 using ST-Link CLI. I've tried -w8, -w32 and -P commands, but every time utility returns error. STM32 ST-LINK CLI ...

Eugene S. by Associate III
  • 777 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.