STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

2 Timers use with stm32F746BG

Posted on September 05, 2017 at 04:58Hello, I use MDK-Lite 5.23 uVision / stm32F746BG. I work with two timer interrupts at the same moment: TIM1_UP_TIM10_IRQHandler(void) + TIM2_IRQHandler(void) + program code at the main() function  void TIM1_UP_TI...

IR diode connection

Posted on September 13, 2017 at 11:35The following circuit was pointed out on a local electronics forum:I mean, it *may* work, under certain circumstances... nonsense nevertheless.One of the comments was, that it nicely complements Cube... ;)JW

0690X00000608COQAY.png

STM32L496 USART1 RX crash @ 1.8V IO

Posted on September 12, 2017 at 10:50Dear community.I have a very interesting issue - I am working on STM32L496 Nucleo board and working with USART1.  Everything works fine there with USART1 receive/transmitting in INT mode.  (Nucleo runs 3.3v with ...

john chen by Associate II
  • 3242 Views
  • 6 replies
  • 0 kudos

SDIO (SDMMC) and FatFS with CubeMX

Posted on May 12, 2016 at 13:55Hello! I try to use the SDMMC1 interface together with FatFS. Initialization is created with CubeMX. My init is something like this: ... MX_LTDC_Init(); MX_SDMMC1_SD_Init(); MX_FATFS_Init(); ... Then I try to use the S...

dennis23 by Associate II
  • 2563 Views
  • 3 replies
  • 0 kudos

DMA delay caused by Interrupts?

Posted on September 04, 2017 at 12:33 On my STM32F411RE I send data to my SPI2 peripheral port using DMA and it works fine, but the moment I enable any kind of interrupts for the NVIC it completely scrambles up my stream of DMA data on my SPI2 -...

Resolved! Should USARTx->BRR have to re-calculate ?

Posted on September 11, 2017 at 16:33 Hi, Now I'm trying to implement UART function as the below, But the problem is keep showing in RS232 Tool. I'm just referring fully reference posting such as https://community.st.com/thread/19577?comment...

0690X000006044uQAA.jpg 0690X000006041cQAA.jpg

Resolved! CubeMX for F0 has no GPIO settings

Posted on May 12, 2017 at 02:33Using recently updated (app and all libraries) CubeMX v4.21.0 on Windows 10, I create a new project for the NUCLEO-32 (STM32F042K6T6) board, but there are no settings for configuring the GPIO pins.When I go to the 'Con...

dale by Associate III
  • 3611 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.