STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI RXONLY with DMA possible?

Posted on August 25, 2017 at 15:30I'm planning to use a STM32L432KC to read 18-bit transmission from an external slave device. It seems the RXONLY master mode is a perfect match for this since it is outputting a continous SPI clock. I could set the ...

STM32F0x devices and HTTPs client

Posted on September 14, 2017 at 13:48(I don't know if i write the post in right sub-forum place).I face to one issue to get data from one server using port 443. HTTPS for getting data instead HTTP. (First at all , I am newbie with secure connection ...

Use SPI DMA with FIFO

Posted on September 14, 2017 at 13:40I'm trying to use SPI DMA with FIFO to read a ADC. The working procedure of my code is as below:ADC give a interrupt to inform the data is ok to read, then we kick start the SPI DMA to read 16bits x 4 (4 half wor...

0690X00000608DIQAY.png

bug in HAL I2S Full Duplex STM32Cube_FW_F4_V1.16.0

Posted on September 06, 2017 at 09:30I'm using I2s2 and I2s2ex in Full Duplex  mode,set the DMA in DMA_CIRCULAR mode,but  HAL_I2SEx_TxRxCpltCallback can't be called,so I modify as follows.Is this a bug?static void I2SEx_TxRxDMACplt(DMA_HandleTypeDef...

sea trix by Associate
  • 1293 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F105 nested interrupt with CAN

Posted on September 13, 2017 at 15:31Hi Community,i have a question regarding to the nested interrupt function of the F105. My Situation: I have 3 Interrupts with different prioritiesCAN bus rx has the lowest priority (highest number) and i want to...

Product Status STEVAL-ISV002 Solar Inverter

Posted on September 14, 2017 at 06:02For the lack of a more fitting category I'll post my questions here1. the schematics for isv002v1 seem to be incomplete, the driver section for the synchronous rectifier is missing (PWM3 - G3, PWM3N - G3N). And I...

mjs by Associate
  • 1178 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.