2017-09-06 12:30 AM
I'm using I2s2 and I2s2ex in Full Duplex mode,set the DMA in DMA_CIRCULAR mode,but
HAL_I2SEx_TxRxCpltCallback can't be called,so I modify as follows.Is this a bug?
static void I2SEx_TxRxDMACplt(DMA_HandleTypeDef *hdma)
{ I2S_HandleTypeDef* hi2s = (I2S_HandleTypeDef*)((DMA_HandleTypeDef*)hdma)->Parent;/* if DMA is not configured in DMA_CIRCULAR mode */
if((hdma->Instance->CR & DMA_SxCR_CIRC) == 0U) { if (hi2s->hdmarx == hdma) { /* Disable Rx DMA Request */ if (((hi2s->Instance->I2SCFGR & SPI_I2SCFGR_I2SCFG) == I2S_MODE_MASTER_TX) ||\ ((hi2s->Instance->I2SCFGR & SPI_I2SCFGR_I2SCFG) == I2S_MODE_SLAVE_TX)) { CLEAR_BIT(I2SxEXT(hi2s->Instance)->CR2,SPI_CR2_RXDMAEN); } else { CLEAR_BIT(hi2s->Instance->CR2,SPI_CR2_RXDMAEN); }hi2s->RxXferCount = 0U;
if (hi2s->TxXferCount == 0U)
{ hi2s->State = HAL_I2S_STATE_READY;HAL_I2SEx_TxRxCpltCallback(hi2s);
} }if (hi2s->hdmatx == hdma)
{ /* Disable Tx DMA Request */ if (((hi2s->Instance->I2SCFGR & SPI_I2SCFGR_I2SCFG) == I2S_MODE_MASTER_TX) ||\ ((hi2s->Instance->I2SCFGR & SPI_I2SCFGR_I2SCFG) == I2S_MODE_SLAVE_TX)) { CLEAR_BIT(hi2s->Instance->CR2,SPI_CR2_TXDMAEN); } else { CLEAR_BIT(I2SxEXT(hi2s->Instance)->CR2,SPI_CR2_TXDMAEN); }hi2s->TxXferCount = 0U;
if (hi2s->RxXferCount == 0U)
{ hi2s->State = HAL_I2S_STATE_READY;HAL_I2SEx_TxRxCpltCallback(hi2s);
} } }else
{
if (hi2s->hdmarx == hdma)
{
hi2s->RxXferCount = 0U;
if (hi2s->TxXferCount == 0U)
{
hi2s->State = HAL_I2S_STATE_READY;
HAL_I2SEx_TxRxCpltCallback(hi2s);
}
}
if (hi2s->hdmatx == hdma)
{
hi2s->TxXferCount = 0U;
if (hi2s->RxXferCount == 0U)
{
hi2s->State = HAL_I2S_STATE_READY;
HAL_I2SEx_TxRxCpltCallback(hi2s);
}
}
}
}2017-09-14 3:04 AM
Just discovered STM32Cube_FW_F4_V1.16.0 has broken our product. A STM32F407 processor is communicating with a MAX9860 codec via full duplex I2S using DMA with circular addressing. It worked well, but updating the HAL library has broken it badly. The problem that HAL_I2SEx_TxRxCpltCallback will never be called from I2SEx_TxRxDMACplt. It is a bug or omission in the HAL code. There is no mention in the release notes that circular buffers cannot be used with i2s DMA.
Also, when using circular addressing it is good to have a HAL_I2SEx_TxRxHalfCpltCallback function as well. Allows for easy seamless i2S transfer using DMA with minimal time constraints.
So we have to revert back to STM32Cube_FW_F4_V1.13.0 or modify HAL.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.