STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C communication issue using LL libraries

Posted on November 23, 2016 at 05:57Hello All, I'm struggling with I2C communication with L476 using LL libraries. In my custom board, a OV5642 camera is connected with I2C1 and a LSM6DS3 IMU with I2C3. Previously I've configured I2C RTC with L151 (...

rumlyen by Associate II
  • 5294 Views
  • 5 replies
  • 0 kudos

What is tsc shield in CubeMX?

Posted on September 22, 2017 at 10:25 I am developing a touch program with STM32F051K8, but have a problem: What is tsc shield in CubeMX? And how to config? thx http://image17-c.poco.cn/mypoco/myphoto/20170922/16/1877216122017092216204jpg?1039x...

Ricky S by Associate II
  • 2279 Views
  • 3 replies
  • 1 kudos

STM32l052R6 Touch-Lib (HAL_TSC) with CubeMX

Posted on June 12, 2015 at 14:58Hi guys, I got problems including some TouchPads with the ''transfer acquisition principle'' with a STM32L052R6 and the CubeMX-generated HAL_TSC library. I couldn't find an example code or a evaluation board, from whi...

How to debug TSC?

Posted on September 27, 2017 at 04:43I porting a tsc sample from \STMicroelectronics\STM32F0xx_STMTouch_Lib_V1.1.0\Projects\Examples\STM32F0518_Ex01_3TKeys_EVAL to my STM32F051 project with touch channel IO using PA0/PA1 and PA3 as samplingIO, but i...

Ricky S by Associate II
  • 845 Views
  • 0 replies
  • 0 kudos

St Link Utility : writing a new external loader

Posted on June 06, 2017 at 08:42Hello,,I need to write (or modify) a new External flash loader for StLink utility.I'm using a STM32F475RCT6 with a N25Q128A13EF840E Quad Spi Flash.It's seems to be very similar to the example given with StLink Utility...

Resolved! STM32H743 possible bug, or two :)

Posted on September 22, 2017 at 15:55Hi, All!I have made a board with STM32H743 (ES32H743 rev.Z datecode 633) and ported quite a big STM32F746 project to STM32H743. The works is not yet finished, but I have some questions and information that can be...

How to optimise the power computation

Posted on September 26, 2017 at 11:58 Hi there, I'm working on STM32F103 MCU and i need to compute the powerof a value. I use the math.h library but I'm looking for a more optimised library, if it's exists. Is there a better way to compute th...

Fede Rico by Associate III
  • 7767 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.