STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Initialize STM32f407 Ethernet without using libraries

Posted on September 21, 2017 at 17:03Hi.Is there any procedure available that shows the steps involved in initializing the Ethernet. The cube code generated uses libraries like HAL. I would like to do this without using these libraries. Is there a p...

STM32 L452 : Programming using SWD interface

Posted on September 29, 2017 at 07:03Hello everyone,I am working with STM32 L452 microcontroller. I'm trying to program this using SWD interface on ST link debugger of the Nucleo board. I am powering the L452 MCU via two different methods :1) Using ...

0690X00000608NSQAY.png

Equivalent part

Posted on September 29, 2017 at 07:05Please share the equivalent STM32 ultra low power MCU for the below requirement: Flash Memory size [KB] 128 SRAM size [KB] 8 Speed [MHz] 32 DMA controller Yes Communication Peripherals [UART, SPI,I2C]:3 - UART, ...

PK K by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos

How can use STM32F429 Discovery Kit?

Posted on September 19, 2017 at 09:01I am new user of stm32f429 discovery kit(STM32F429ZIT6).I have some querry as below:1).Which software/IDE should i use for programming?.2).Any sample code to interface OV9655 camera with this kit?3). How should i...

How to use Timer to watch the external input signal?

Posted on September 29, 2017 at 07:10Hi,I'd like to implement such as IWDG without reset. Especially, I want to watch the one external input signal but it with limited time. So what If one external signal is toggling in defined time, no response but...

Proper sequence to configure I/O to AF mode

Posted on September 28, 2017 at 22:38I think this question relates to STM32 in general, but specifically the part in currently working on is a STM32L051. After stopping the CPU to stop mode, with I/O reconfigured is analog inputs to save power, I'd ...

Resolved! STM32L432 - User Data Flash Write

Posted on February 10, 2017 at 18:44 Hi, I am new to this forum so bearwith me. We are attempting to store user data in flash on STM32L432 for things such as calibration values for different sensors or CAN ID's so that these values don't ne...

Nolan L by Associate III
  • 7071 Views
  • 10 replies
  • 0 kudos

Connect to WPA2 network using micropython

Posted on September 28, 2017 at 18:42 I'm a noob and I actually have two problems. First, I'm trying to connect a SPWF04SA board to a WPA2 protected network using micropython. From some examples I have found on the micropython website it looks...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.