STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 vs. STM32L4+ prices discrepancy

Posted on November 20, 2017 at 17:26Hi,   I wonder why the STM32H7 distribuitors prices are so much higher than ST prices for 10K units compared to others STM32 devices. Ex:  STM32L4R7VIT6   ST price for 10K = U$7.80     and Distribuitors minimum pr...

Asantos by Senior
  • 1289 Views
  • 2 replies
  • 0 kudos

STM32F302 using TIM in output compare

Posted on November 20, 2017 at 13:41I'm using STM32F302 Nucleo board and I'm trying to configure TIM1 in such a way that it will output a 12 us long pulse on its output.I've configured TIM1, GPIO port C with its appropriate alternate functions as we...

Using the RTC

Posted on March 20, 2015 at 14:12 I'm having issues making the RTC work as expected. This is the code which is called periodically: RTC_TimeTypeDef currentTime; HAL_RTC_GetTime(&hrtc, &currentTime, FORMAT_BIN); char uartMsg[32...

dscdsc by Senior
  • 7262 Views
  • 16 replies
  • 0 kudos

STM32H743I Eval Board Schematic for SD card

Posted on November 13, 2017 at 05:01Hi,We are planning on using the STM32H753 in our design. We currently have the STM32H743 eval board with us and we have the following query regarding the sd card schematic on the user manual 'UM2198'.Qn.:  The sd ...

strlen flash writing question.

Posted on November 20, 2017 at 03:04 In the flash memory as shown in the following code, the str1 and str2 values are divided into 4 bytes I want to write down. I have an error like the image I captured .; When I have an event, I write it to Fla...

0690X0000060PFSQA2.png

STM32F765 MCU Nand flash issue

Posted on November 20, 2017 at 07:45I am working on STM32F765BIT MCU with our custom board . In our board NAND flash is connected to Bank3 (0x80000000 - 0x8FFFFFFF). I configured using STM cube and just tried to read device ID but MCU is getting loc...

How can SPI Master ReceiveData from SPI Slave ?

Posted on November 18, 2017 at 19:32 Sorry about my english.Hi everybody . I'm using SPI slave sendata to SPI master. But it not working. I'm using SPI2 to mode slave and SPI1 to mode master . It's my project: /*.......main.c.......*/&sharpinclude ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.