STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to apply 74HC165 for STM32

Posted on December 26, 2017 at 15:08 Dear community, I can hardly find any code for the STM32 using a parallel in/serial out 74HC I managed to program the stm32f103c8 to work with a 74hc595 which is the counterpart, so it's a serial in/parallel o...

why does ADC_FLAG_EOS get called after each channel?

Posted on April 06, 2017 at 12:22 Hi I am trying to use the ADC in the STM32L07 as a multichannel scan. I have set up Cube for 3 analogue channels, AN0, Temperature and VRef Int. I have set it up for single scan usign the HAL_ADC_Start_IT(&hadc);...

Does ST have multi connection TCP/IP reference design?

Posted on December 28, 2017 at 14:19Right now the HTTP/Netconn code is replaced with TCP/IP echo server using the sockets API. It 's the typical architecture of a listener thread that spawns connection-handler threads. When we exercise more than one...

EHD by Associate II
  • 1092 Views
  • 1 replies
  • 0 kudos

STM32F429

Posted on December 28, 2017 at 08:01Hello Sorry for disturb and sorry if its not the right forum to ask this we use the example that provded with discovery  stm32f429  DMA2D we want to put a bitmap ; but in that example we see that the bitmaps are c...

IAP for STM32F030C8 using HAL library

Posted on December 28, 2017 at 10:32I want to write IAP for STM32F030C8. I have searched through the web but found the application using Standard peripheral library. Is there any application that is developed with HAL library? Also there is no provi...

shrek T by Associate
  • 1111 Views
  • 1 replies
  • 0 kudos

problem with use HAL_FLASH_Program

Posted on March 05, 2015 at 09:08when i use this function uint8_t    Save_data(void) {     uint8_t    idx;     uint8_t    addr;     FLASH_EraseInitTypeDef    erase;     uint32_t    pg_error;     HAL_FLASH_Unlock();     erase.NbPages = 1;     erase....

Has anybody converted the PWM frequency and duty cycle measurement exmaple from the STM32CubeMx examples to use STM32CubeMx to configure the hardware (.ioc file to configure the timers)?

Posted on October 10, 2017 at 21:17The 'STMCubeF2\Projects\STM32F207ZG-Nucleo\Examples\TIM\TIM_PWMInput' example configures the timers with direct calls to the HAL.I am trying to keep all of the pin allocation and resource initialization within STM3...

Mike Katz by Associate II
  • 5110 Views
  • 11 replies
  • 0 kudos

Independent WatchDog

Posted on December 28, 2017 at 09:12We are using Independent WatchDog in our system configured for every 2 seconds. The intention is that if the Refresh is not happening for every 2 seconds, the software will be resetted.   But, what is observed is ...

Anand A by Associate III
  • 798 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.