STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

why does Led blink modify in this code?

Posted on January 06, 2018 at 14:42hi.i wrote a code in IAR for stm32f103ret, the code is for blink led and  problem is the time is different when the led is on and the led is off .But the wait is same both of set led and reset led.19 seconds led is...

synchronous non-multiplexed PSRAM

Posted on December 21, 2017 at 13:34We are using STM32 microcontrollers that have a parallel data bus driven by on-board memory controller called FMC. This data bus has multiple operating modes and the one in which we are interested is synchronous n...

AC DIMMER WITH STM32F373

Posted on December 24, 2017 at 22:48hello i am working on AC dimmer with stm32f373.i have a issue when the fire angle change in TIMx->ARR.in this case the lamps have filkcer.i use the timer of MCU that runs in timer mode with internal clock.how can ...

l90mehdi by Associate II
  • 3315 Views
  • 6 replies
  • 0 kudos

STM3210C-Eval BNC channel11 analog input

Posted on January 08, 2018 at 09:51Hello, I am looking for example of how to get analog data from BNC (channel11) instead of potentiometer in STM3210C-Eval board. I used the peripheral library example ADC1 DMA as a base. I understand that PC.04 (GPI...

Hello am working on STM32L476RG development Board i am trying to develop a smart watch as part of my masters academic project when trying to import the code from mbed complier the code is compiled but it is not being dumped may I know the reason for it

Posted on January 06, 2018 at 18:29 Hello am working on STM32L476RG development Board i am trying to develop a smart watch as part of my masters academic project when trying to import the code from mbed complier the code is compiled but it is not b...

CAN and system clock configuration

Posted on April 26, 2017 at 06:50Hi, CAN interface  on STM32F769I is not sending data using Clock configuration 1 but CAN interface is sending data with configuration 2. I am not able to narrow down that how the CAN interface is getting affected by ...

Jith cr by Associate II
  • 1820 Views
  • 3 replies
  • 0 kudos

Resolved! H743 ._user_heap_stack in D2 section causes Hard Fault

Posted on January 03, 2018 at 22:16Hello.Why is it not possible to point the ._user_heap_section in the D2 RAM section?A tiny project based on SW4STM32 for NUCLEO-H743ZI is attached.I just modified the linker script to have _user_heap_stack in D2 an...

STM32f030rc AES Encryption

Posted on January 06, 2018 at 08:21Hello everyone,I am using STM32f030rc for my application. In which I want add 128bit AES encryption. For that I am referring STM32_Cryptographic _Examples. I have taken functions from AES128_CTR file. In which I am...

How do I enable UART4 on the B-L475E-IOT01A? It appears that UART4 needs to be defined; but in which header file. What else needs to be done to enable and use the port?

Posted on January 07, 2018 at 06:35I desire to use UART4 to talk to a GPS module over serial communications on an Arduino shield board. To do this I need to use UART4, but it does not appear to be enabled. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.