STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error_Handler debugging

Posted on February 27, 2018 at 19:29Hello,The HAL code uses a Error_Handler() function which just spins forever in a tight loop.   I've seen comments about changing the call to report __FILE__ & __LINE__  which I may do.   But I thought setting a br...

STM32F429 LCD Flickering

Posted on February 27, 2018 at 13:16I use STM32F429 witch display on 7inch LCDThis board's status was normal after display rectangle.but something has problem during display rectangle with some flickering.It has problem that use DMA2D or direct ramb...

Kwon YM by Associate
  • 1525 Views
  • 2 replies
  • 0 kudos

STM32F7 HAL LL Driver Bug

Posted on December 05, 2017 at 16:40I am using the USB FS device with the CDC class. I used STM32CubeMX V4.23.0 with the STM32CubeF7 V1.8.0 add-on. The max packet size is set to 64 bytes and the EP TX FIFO buffer for the EP is set to 64 bytes in USB...

MDS by Associate III
  • 1562 Views
  • 2 replies
  • 0 kudos

Problem using arm_cfft_q15

Posted on February 27, 2018 at 01:32Hello,I am doing a project in which I am using the FFT to do some calculations for a determined signal. I get real data from the ADC and then process it with the FFT.I noticed that the FFt give me an incorrect out...

STM32F446 FatFS Adafruit BSP drivers

Posted on February 27, 2018 at 12:49Hi! I am trying to use an SD card with the STM32F446RE (using Attolic TrueSTUDIO) but I cannot seem to figure out what I am doing wrong. I get this error:FatFS\sd_diskio.h:57:14: error: unknown type name 'Diskio_d...

System reboot without NRST low

Posted on February 27, 2018 at 11:02I'm using an STM32L152 with IAR embedded workbench.This MCU has an external reset pin (NRST) which is bidirectional. The MCU outputs a low signal if its reset system detects a watchdog reset, software reset or low...

Resolved! OTG_HS usage with STM32H753xI

Posted on February 22, 2018 at 15:04Hi,In-fact I tried asking query through service request. The website portal seems to be very slow. I am not sure whether it got submitted or not.So I am asking the query directly to you here. Please help me in add...

Getting string on virtual com port.

Posted on February 26, 2018 at 12:04I'm getting a string from a terminal. int main(void){  Set_System();  Set_USBClock();  USB_Interrupts_Config();  USB_Init();    while (1)  {    if (bDeviceState == CONFIGURED)    {      CDC_Receive_DATA();      /*...

DfuSe Problem with STM32L0 73 on chip usb bootloader

Posted on September 22, 2016 at 18:53Hi,I have a Problem with the DfuSe Demo (v3.05) and the STM32L073CZT  on chip bootloader.It is not possible to upload or down Load from/to the InternalFlash.Downloading or Uploading the DATA Memory is possible. I...

0690X00000604i2QAA.png 0690X00000604vUQAQ.png

ADC fluctuations problem

Posted on February 26, 2018 at 14:50Hi,I am having a problem with ADC read. The values I get from conversion are 100% random. They get from 0 to max range without any pattern. Example codes from MXCube work fine and the value is stable. My own code ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.