STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 UART pull up to 5V on RX

Posted on April 10, 2018 at 17:58Hi all,Checking a schematic of an RX485 transceiver connected to STM32F401 UART, I got into this detail that captured my attention:The RX line is directly connected to the RX pin of UART1 of the the MCU and it is pul...

0690X0000060AVDQA2.png

Sample sfecific ADC channel

Posted on April 12, 2018 at 12:41Hi,I'm trying to work with the ADC of the STM32F072RB which have 1-ADC with 16 channels,what I'm trying to do is to take 1000 samples of ADC_CH1 every X second and take 1000 samples of ADC_CH2 every Y seconds and onc...

Ariel G by Associate II
  • 986 Views
  • 1 replies
  • 0 kudos

Bootloader jump to user code

Posted on April 11, 2018 at 15:22I am able to jump from User code into the built-in bootloader without any issues, I am also able to upload the new .bin file using the UART and ST FLASHER Demonstrator, however when I tick the Jump to user code optio...

STM32F334R8T6 can not read memory

Posted on April 12, 2018 at 10:08I have designed a board with STM32F334R8T6. The STM32 pins are configured as in the attached file (I do not think there is a problem here since I have already used the same configuration without problems). The microc...

NUCLEO-F767ZI CAN bus example

Posted on March 27, 2018 at 12:17Hello, is there a working example for CAN bus on NUCLEO-F767ZI board? I tried to search the STM32F7-Cube and was not successful. Thank you in advance! Vaclav#can-interface #stm32f7

Resolved! Event change state output pin in example TIM_OCToggle

Posted on March 26, 2018 at 12:53Hi, i have implemented the example TIM_OCToggle from stm32f40xx to stm32f103xx, both work fine.I want a event in the moment change state output pin of the channels OC, as occurs in the events:HAL_TIM_PeriodElapsedCal...

Resolved! Migration from STM32F105 board to STM32F411 board

Posted on April 09, 2018 at 08:27Hi every body,Really I need your help in order to see if there are any extra change in the schematic side.Right now I use the same board used for STM32F105 to my new STM32F411.What I did:  - I just change the old mic...

Questions about SystemClock_Config() generated by cubeMX

Posted on April 12, 2018 at 08:23The SystemClock_Config() function is generated by cubeMX in main.c. It configure the different clocks used by the system. The question is that it handles the systick timer count in this way:HAL_SYSTICK_Config(HAL_RCC...

Kefei Yao by Associate III
  • 895 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.