2018-04-11 11:23 PM
The SystemClock_Config() function is generated by cubeMX in main.c. It configure the different clocks used by the system. The question is that it handles the systick timer count in this way:
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
It just divides the Hclk frequency by 1000 (assume the system timer clock is provided by HCLK). This result in 1ms tick regardless the actual value of systick set in the freeRTOS configuration in freeRTOSConfig.h. I assume something like
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/configTICK_RATE_HZ);
should be used.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.