STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Ethernet Port (TCP Throughput)

Posted on May 28, 2018 at 12:09Hi Guys,I am currently performing the TCP throughput Test by using lwiperf framework as provided. I have performed the test on below Nucleo 144 pins board, NUCLEO-F207ZGNUCLEO-F746ZGBoth of the boards are running a mo...

0690X0000060KuHQAU.png 0690X0000060KuIQAU.png
whwong84 by Associate II
  • 1090 Views
  • 0 replies
  • 0 kudos

Mass storage problem with SD card

Posted on May 28, 2018 at 09:52Hello, i am trying to use the mass storage interface with my SD card by the help of the stm32 cube. My mcu is stm32f405 and i'm using SDIO 4 bits + USB full speed stack. I am able to see the device and read all the fil...

issa by Associate II
  • 793 Views
  • 0 replies
  • 0 kudos

USART2 : Communication RS232

Posted on May 17, 2018 at 14:40Hello,I have a prototype where a sensor send information in RS232 to my STM32152RE board through a MAX232 to convert the signal. I plugged in my board with RX/TX on USART 2 (+5V et GND).I used CUBE MX and i only modify...

How to use X-CUBE-AVS 1.0.1 for 32F746GDISCOVERY (STM32F746NG MCU), which is has hex file for 32F769IDISCOVERY ?

Posted on May 09, 2018 at 13:45I have 32F746GDISCOVERY (STM32F746NG MCU) board and wanted to use Amazon voice service on it. But the X-CUBE-AVS  1.0.1  program present on STM website is for 32F769IDISCOVERY board. Also it contains the binaries and h...

Reasons for TIM CCx ISR not firing on STM32L433

Posted on May 25, 2018 at 15:57Hi there,I have a rather odd problem and am trying to find a solution or reason for it:I am using 3 different timers on STM32L433 with 4 capture compare registers each to generate a total of 12 completely independant s...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.