STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CS43L22 analog passthrough

Posted on July 19, 2017 at 13:28Can anyone help me with using the codec CS43L22 in analog passthrough mode on STM32F4-Discovery.Flow of applicationAnalog Input ---> ADC ---> DAC ---> CS43L22 ---> Headphone or SpeakerI have got ADC and DAC working, b...

aditya by Associate II
  • 4826 Views
  • 4 replies
  • 0 kudos

Changing stm32L4 clock speed to 26 Mhz

Posted on June 03, 2018 at 01:41Hello, I just want to make sure what I'm doing is right. I'm using MBED and stm32L4. I want to change clock speed to 26 Mhz, I plan to use MSI as input.  In order to do so, I will change the parameter PLL_M and leave ...

GPIO strange behaviour STM32F427

Posted on June 04, 2018 at 19:39Hello,i have a simple code where i just init some GPIO ports on a STM32F427VI  ( 100pin package).The application controls via pin PA8 some transistor which switches on/off a relay after some delay...I have noticed  if...

Bogdan by Senior
  • 1431 Views
  • 2 replies
  • 0 kudos

reference schematic file for F429I Discovery board

Posted on June 04, 2018 at 02:14for most of the other boards I have looked at, the downloads section contains a 'schematic' package with the altium designer *.schdoc files for the board. The F429I discovery board schematic download only has the PDF ...

Garbage Printing after wake up from STOP 2 mode - stm32l476rg

Posted on June 04, 2018 at 09:21Hi, We are working on STM32L476_NUCLEO board. We successfully entered and exit from STOP 2 mode upon RTC timer expiry. However, when we print a message after wake up, garbage is printed. Here is the code. print ('Goin...

H UQ by Associate II
  • 2827 Views
  • 5 replies
  • 0 kudos

14 bit DCMI with Boson camera

Posted on June 03, 2018 at 21:30Hi I am using the DCMI on STM32H743 in 14 bit mode  with a 16 bit camera but I am only use the 14bits MSB  but I only get 8 bit through the system .if I change to 12 or 10 the same again only the first 8 bits but a im...

Resolved! Stm32F746g-disco LTDC-FMC

Posted on June 02, 2018 at 23:49Hello! I'm trying to run an LCD installed on the board Stm32F746g-disco, memory and the display are successfully initialized, but I can not fill the display with color. What is wrong in my project? Maybe someone has a...

Hosting by Associate III
  • 5024 Views
  • 10 replies
  • 0 kudos

Alternate DMA I2C with normal operation

Posted on June 04, 2018 at 15:59I'm trying to rewrite the I2C gyro (MPU6050) read operation of an STM32F0xx based flight controller (https://github.com/silver13/BoldClash-BWHOOP-B-03) to partially TIM_Update/DMA based I2C readout for accurate loopti...

Resolved! ADC pin configuration in STM32F072B

Posted on May 30, 2018 at 14:36How to configure ADC pin in STM32F072B controller?I do not give any input in ADC pin but I got the output? Same configuration and code working correctly on STM32F072B Discovery Board.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.