2018-05-30 5:36 AM
How to configure ADC pin in STM32F072B controller?
I do not give any input in ADC pin but I got the output?
Same configuration and code working correctly on STM32F072B Discovery Board.
Solved! Go to Solution.
2018-06-04 12:25 AM
Hello,
Schmidt triggers are disabled automatically once you configure IO line in analog mode.
Best Regards,
Artur
2018-05-30 5:45 AM
Hello,
In case you are using STM32CubeMX tool:
If you would like to select IO pin as analog (to be used by ADC), please just select ADC channel. You can configure all not used pins automatically as analog using Project settings. The second option is used to reduce current consumption in the application as by default IOs are configured as input floating. In this configuration there is Schmit trigger active at the pin which is causing an additional current consumption. This component is disabled in analog mode.
In case you are writing code manually you should configure IO lines in analog mode (GPIOx_MODER register).
Best Regards,
Artur
2018-05-30 6:38 AM
Thanks to the for the reply.
Yes, I am using STM32CubeMX tool.
I check analog pin configured is correct. but how to disabled Schmit trigger?
2018-05-30 6:45 AM
That does not mean too much.
What is the external wirings on both boards ?
Short the ADC input to ground, and you shall read zero. If the input floats, the S&H will pick up noise.
2018-05-30 11:26 PM
Thanks to the for the reply.
Yes, I am using STM32CubeMX tool.
I check analog pin configured is correct. but how to disabled Schmit trigger?
2018-06-04 12:25 AM
Hello,
Schmidt triggers are disabled automatically once you configure IO line in analog mode.
Best Regards,
Artur
2018-06-04 6:31 AM
Hello,
Thanks for the sharing the information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.