PID controller
Posted on June 05, 2018 at 16:44i would implement PID controller in my card nucleo stm32f446re.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on June 05, 2018 at 16:44i would implement PID controller in my card nucleo stm32f446re.
Posted on May 30, 2018 at 05:26I'm developing USB MSC features with chip STM32F779 using SD Card .Now I can read/write/format data in SDcard. But there is 1 issue is I can not do Safe Eject the USB from Window. Window said that the device is “safe t...
Posted on June 05, 2018 at 16:22Hello,we are trying to decode a jpeg on the STM32F769I-DISCO and display it on the LCD while decoding. For that we modified the JPEG example JPEG_DecodingUsingFs_DMA a little bit. Here is the important part of code:un...
Posted on June 06, 2018 at 10:48Hello, I made a model NUCLEO-L053R8 card containing modules X-NUCLEO-IKS01A1 and X-NUCLEO-IDS01A4. Now,I want to switch my program used for the NUCLEO card to another project, that of my prototype which containing a S...
..
Posted on June 06, 2018 at 10:22I have CDC HOST. (stm32f205)It is work normal, but when i connect to this same device(CDC Device (stm32f303 )) i can get a problem with enumeration. It is if device in resert or not started normaly. In this case HOS...
Posted on June 06, 2018 at 07:09From where can I download I-CUBE-LRWAN v1.1.2? The current version is 1.1.5 but I need v1.1.2
Posted on May 31, 2018 at 15:05I want to use I2C fast mode(400KHz) and USB full speed mode in parallel. My controller is STM32F103VCT6. In reference manual I had read that for USB we must use 48MHz clock and also for I2C fast mode communication i2c...
Posted on December 06, 2016 at 01:14Excuse me.I want to get data about STM32 hands-on workshop.(such as presentation file, pdf, sample codes)I don't attend off-line hands-on workshop.So, I want to see a relevant data about hands-on workshop.Let me k...
Posted on February 13, 2018 at 13:22HiI'm having quite an issue while using the FatFs on a SD card.I configure everything on the Cube following this tutorial :https://www.youtube.com/watch?v=kRhF44v2ezM I'm kinda lost, and i would like some support...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.