STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to use Uart RTO IT for TX?

Posted on June 15, 2018 at 16:44Hi,I'm working on an UART thing on STM32F0XX. I already successfully use IT for reception and for timeout on reception, but now I need to use the RTO (timeout) feature to detect the timeout after a transmission and ca...

stm32f407 center aligned PWM with phase shift

Posted on June 17, 2018 at 15:29Hello everyone.I'm using STM32F407 Black VET6 board. I need to create 6 center-aligned synchronized PWM signals with the same frequency, but every signal needs to have its own DutyCycle and PhaseShift control. Example...

0690X0000060BebQAE.png

pwm with dma

Posted on June 19, 2018 at 10:09HiI am trying to make a sinusal variable freq  wave with dma And pwm . but i cant set  a timer for trigger the dma in cube . please help me to set the cube for it . i use nucleo-f746zgthanks best regurdp m : excusme f...

UART never in ready state for transmit function

Posted on June 19, 2018 at 07:41I am trying to include UART into a sample program without using cubeMX. To my knowledge I have added everything it needs, but when I get to the transmit command, it checks the statement:huart->gState == HAL_UART_STATE...

Reset ULP bit after stop (STM32L1)

Posted on May 14, 2018 at 21:30After I upgraded my application from mbed 5.4.7 to 5.7.7, my comparator is unreliable after a STOP. Basically, this is how the MCU is put into sleep (from https://github.com/ARMmbed/mbed-os/blob/master/targets/TARGET_S...

S2LP MISO high at random

Posted on June 19, 2018 at 09:35Hello, I have an issue with my custom pcb with stm32l476rg and S2LP integrated circuit. I have succesfully ported and run the firmware using nucleo L4 and FKI868V1 board. Still have some troubles with running it on pc...

stm32f745n availability

Posted on June 19, 2018 at 09:12Hello,Browsing the STM32F745 DS I saw that there is a 216pin option marked in the partnumber with the letter N.When I was looking at the ST website as well as digikey and other sites to try and buy it I couldn't find ...

eli_az by Associate II
  • 649 Views
  • 0 replies
  • 0 kudos

Question about CAN2 reactivation after connection lost

Posted on June 19, 2018 at 08:54Hello.I am developing on stm32f4discovery board and I use both, CAN1 and CAN2 in my project. I know that CAN2 can't be used without CAN1, but what I am struggling to figure out is that if for example, I lose physical ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.