STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L451 strange RTC issue

Posted on July 11, 2018 at 17:03I'm curious if anyone else has seen this issue.We are using 20 ppm LSE at 32768hz as the clock source for our RTC.  Over an 8 hour period, we are a few seconds off vs. the expected max of .6 S for the 20 ppm.Our syste...

mhage by Associate II
  • 1829 Views
  • 3 replies
  • 0 kudos

4 bit SDIO doesn't work although 1 bit SDIO works SDCARD

Posted on January 18, 2018 at 14:37 Hey everyone, I have a quick question concerning the 4 bit sdio sdcard implementation. The 1 bit sdio seems to work perfectly. I have absolutely no issues, although when implementing 4 bit it completely bugs ou...

con3 by Senior
  • 16049 Views
  • 15 replies
  • 1 kudos

Question regarding hardware state and debug in stop mode

Posted on July 11, 2018 at 01:56Hi,I am currently writing a program for the part STM32L031F6.  I am using StopMode to put the uController to sleep.I have a couple of questions I was wonder if you could help.1. When waking up from stop mode, do I nee...

Vu.Andy by Associate III
  • 2766 Views
  • 2 replies
  • 0 kudos

HAL_SPI_Transmit/HAL_SPI_TransmitReceive timeout

Posted on July 11, 2018 at 20:13Hi,I used to have the SPI1 working connected to MAX31865 breakout board. For some reason it's not working at all now. I traced into the code, seems HAL_SPI_Transmit() failed on __HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXE) u...

0690X0000060M7uQAE.png

Trouble entering STOP2 on stm32l432

Posted on July 09, 2018 at 15:06I'm having trouble entering stop2 -- instead of going to stop2 my code seems to enter sleep; this is based upon measuring power levels -- I have the RTC fed by an external crystal and a 1 second interval alarm.  I can...

VBAT for RTC backup

Posted on October 10, 2016 at 13:12Hello, should i connect 3V battery to Vss or Vssa for RTC backup (external 32768 resonator)? #too-vague #stm32-vbat-rtc

mailbox by Associate II
  • 2883 Views
  • 5 replies
  • 0 kudos

EXTI9_5_IRQHandler missing in CubeMX H743i_Eval Build

Posted on July 07, 2018 at 01:39Trying to figure out reasons why a CubeMX build cannot replicate the functionality of the repo application:STM32Cube\Repository\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Applications\FatFs\FatFs_uSD_DMA_RTOS.The...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.