STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube MX 4.25.1 for Download

Posted on July 11, 2018 at 21:21Does anyone have Cube MX 4.25.1 available for download?4.26 does not work. 4.25.0 does not work either and I have 4.24.Thanks,

Difficulty interfacing DS2482 & DS18b20 with STM32F4

Posted on July 06, 2018 at 13:26Hello,I am working on STM32F4 discovery board, trying to interface DS2482-100 (I2C driver ic) and DS18b20 (Temperture sensor one wire).my interface is likestm32f4 ---i2c---> DS2482-100 ----one wire----->DS18b20 I am a...

Resolved! STM32F746 - SPI sends twice problem

Posted on July 11, 2018 at 11:43The original post was too long to process during our migration. Please click on the attachment to read the original post.

M G_2 by Associate III
  • 4343 Views
  • 5 replies
  • 0 kudos

Resolved! pwm and time based interrupt

Posted on July 10, 2018 at 13:42Hi all,I am working on STM32F746G - DISCO. I have started working with STM32 just recently, sorry if this is a silly question. I need to use 1 timer to get PWM output from one of its channels, and generate time based ...

Den In by Associate II
  • 3907 Views
  • 4 replies
  • 0 kudos

[STM32F303RETx] I2C not working reliably with CAN enabled

Posted on July 12, 2018 at 17:07Hi All.We are using the MCU as the I2c-master, and a MPU6050 as the slave.Following are the I2C-parameters of the MCU (from Cube) :I2C Speed Mode                           :     StandardI2C Speed Frequency (KHz)      ...

STM32L151RBxA UART1 not working

Posted on March 03, 2017 at 16:48Hi all,I am trying to enable UART1 on stm32l151RBXA controller. I am using code generated by Cube. I tried modifying the code but serial port just does not work. I am only trying to send text to serial port but this ...

nps by Associate II
  • 2320 Views
  • 4 replies
  • 0 kudos

Resolved! Program several STM32H7 in one shot

Posted on February 27, 2018 at 16:16Hello,I am working on a board that has three STM32H7 on it. They are running exactly the same code.  It is really boring and time consuming to flash them one by one...I would like to know if there is a standard wa...

Geo En by Associate III
  • 1660 Views
  • 2 replies
  • 0 kudos

USB Host MSC

Posted on July 12, 2018 at 15:40Hi all,I'm trying tho get a USB flash drive working in USB host mode. I'm using an STM32F105RCT chip which I have mounted on a Nucleo F103RBT board.The chip is working an I can program it, will respond on the USART ch...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.