STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

syntax is the bane of my work...

I don't understand why this would compile and work for one project but not another...const char Menu[40][32] = { "\033[91;2mShow Menu\033[93;2m <space>", "\033[0m ", "1 Read Flash status" };   char * ptr = &Menu; <- fails here [C...

T J by Lead
  • 1841 Views
  • 4 replies
  • 0 kudos

SPI master send simle data error

Hi, do you know how is the simplest code to send data from stm32(master) to arduino (slave) through spi.I tried to write my own code, so here is the sktech ofmy code :#define SPI2_Funct 0x05 // This is a function of GPIO AFR#define CMD_LENGTH  2#defi...

STM32H753I-EVAL SDMMC cubeMX problem

Hello, I am a total newby for what concerns stm32 programming and this question may be stupid.... I am using a STM32H753i-eval board and will need to use fdcan, lcd, SD and a few more peripherals. For this reason I started my project using STM32cubeM...

gian666 by Associate II
  • 2891 Views
  • 6 replies
  • 0 kudos

Basic question regarding timers and generating a simple delay

Hi there,Let say I want to generate a 1 ms delay using a timer. I set my prescaler to have a 1ms granularityTIMx->PSC = (uint16_t)((SystemCoreClock / 1000U) - 1);Now if I want to generate a 2ms delay I usually do it like this (assuming the UIF flag i...

Kraal by Lead
  • 1146 Views
  • 2 replies
  • 0 kudos

STM32F746-Disco SDRAM problem

Hi,I have problem with the test of SDRAM memory. I use STM32F746 Discovery kit where is MT48LC4M32B2 memory.  SDRAM size is 128-Mbit SDRAM but only 64-Mbit is accessible on kit. So I try to test the entire 8MB SDRAM memory. Unfortunately, when the la...

MPeco by Associate
  • 1092 Views
  • 1 replies
  • 0 kudos

STM32L496 I2C1 PA9 PA10 stuck low

Posted on June 06, 2018 at 12:49I am having problems configuring the I2C1 gpio pins on the STM32L496 on pins PA9 and PA10.After the gpios are configured the SCL and SDA lines go from a high level to a low level, which is unexpected. After configurat...

Problem with STM32 Cube MX 4.26.0

Posted on June 08, 2018 at 21:13The problem found in STM32 Cube MX 4.26.0, is that the tool over-wrote thefiles of my project..I'll describe what happened:1. My project I was working on was created with STM32 Cube MX 4.25.0..2. I updated the STM32Cu...

0690X0000060LCKQA2.png 0690X0000060LCZQA2.png 0690X0000060LCeQAM.png

Resolved! Reading the H7 temperature sensor calibration parameters

Posted on June 28, 2018 at 18:34STM32H743To improve the accuracy of the temperature sensor measurement, each device is individually factory-calibrated by ST. The temperature sensor factory calibration data are stored by ST in the System memory area,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.